Skip to main content
lyoy
Associate II
March 9, 2022
Question

What is going on with this PWM output timer 2?

I am following this tutorial and trying to get a complete understanding of the code:

https://embedded-lab.com/blog/continuing-stm8-microcontroller-expedition/6/

I have a few questions regarding the TIM2_setup(void) function:

1 Why is channel 1 and channel 2 used in identical fashion like this? Might this be to use the two output pins on the MCU in parallel for higher current capacity?

2 Isn't this line redundant:

"TIM2_SetCompare1(100);"

when the "duty cycle count" was already set to 1000 in this line?

TIM2_OC1Init(TIM2_OCMODE_PWM2, TIM2_OUTPUTSTATE_ENABLE, 1000, TIM2_OCPOLARITY_LOW);

3 Are these two lines effectively the same?

TIM2_OC1Init(TIM2_OCMODE_PWM2, TIM2_OUTPUTSTATE_ENABLE, 1000, TIM2_OCPOLARITY_LOW);

TIM2_OC1Init(TIM2_OCMODE_PWM1, TIM2_OUTPUTSTATE_ENABLE, 1000, TIM2_OCPOLARITY_HIGH);

If not, why would PWM mode 2 be chosen here?

    This topic has been closed for replies.