Skip to main content
AG1
Associate II
October 9, 2018
Question

What are the min & max input voltage levels for USBUF01W6 ?

using the USBUF01W6 IC for self powered USB device with full speed connection

Can i give 5V DC volt BUS POWER from HOST to it? as it will also be used for pullup on D+ lines

This topic has been closed for replies.

5 replies

FGUIT
ST Employee
November 15, 2018

Dear,

Yes, you can use USBUF01W6 to protect D+ and D-, and also to connect pullup resistor to set low speed or full speed device. Vbus will not be connected to this part, but should be protected by another part, such as ESDA7P120-1U1M.

AG1
AG1Author
Associate II
January 10, 2019

still, what are the min. & max. input voltage levels for USBUF01W6?

AG1
AG1Author
Associate II
January 10, 2019

is there any replacement part for USBUF01W6,

i would like to supply 5V to USB filter IC & it's resistor through the power coming from USB cable i.e. HOST

So device pull up will remain active when VBUS is high

FGUIT
ST Employee
January 15, 2019

Dear,

Min voltage is 0V and Max voltage is 5V, on all pins, in reference to GND.

Pull up should be connected to 3.3V, to set full speed or low speed.

EMIF02-USB01F2 can be used on USB full speed / low speed, it integrates:

  • pull up resistor to set full speed or low speed, to be connected to 3.3V
  • ESD protection on D+, D-, Vbus, ID, 3.3V of pullup resistor
  • RC filtering

AG1
AG1Author
Associate II
June 18, 2019

hi, for USBUF01W6---datasheet shows only 3.3V, & does not have other information

can you share if any other document is available for it