Skip to main content
hsynenko
Associate II
Sep 29, 2010 5:55 AM UTC
Question

What are the differences between Indepent Watchdog and Window Watchdog?

Posted on September 29, 2010 at 07:55

What are the differences between Indepent Watchdog and Window Watchdog?

    This topic has been closed for replies.

    1 reply

    napoleoni.jacques
    ST Employee
    May 17, 2011 1:10 PM UTC
    Posted on May 17, 2011 at 15:10

    Hello,

    Here are some information between Independent watchdog IWDG and Window watchdog WWDG:

    - Independent WD is basically a 8-bit down counter that you presets at the start of the application and regularly refreshes before it reaches 0 value that will start IWDG reset. The timeout can be adjusted from 60µs to 1s. You can refresh it at any time you want on the opposite of WWDG.

    - Window WD must be refreshed during a time limited window, not before and not after this window. It can detect early or late application behavior. Its timeout can be adjusted between 75µs up to 64ms.

    For more information, please read in details the device reference manual.

    Regards.