Skip to main content
Associate III
June 20, 2023
Question

wakeup function

How to use Port D as wake up function after the STMS003

goes to sleep

 

    This topic has been closed for replies.

    6 replies

    AA1
    Senior III
    June 20, 2023

    You have to configure a pin to generate and interrupt and you need the interrupt handler. See RM0016 "External interrupts" and "Power management"

    SRAM.11Author
    Associate III
    June 21, 2023

    Thank you I had find out solution for sleep mode and also found my AWU config wrong I am trying to correct that.Now my sleep mode have been executed but wakeup function not.It may be because of that halt function? when I am running my code in step by step debugger it says program went to halt .

    Peter BENSCH
    ST Technical Moderator
    June 22, 2023

    Have you configured the port pin as an input pin?
    Have you set the interrupt on this port pin to the desired edge (falling, rising) and activated it?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    SRAM.11Author
    Associate III
    June 22, 2023

    Yes in stm8s003f  I couldn't find the EXTIPIN sensitivity but I set it for the port

    Peter BENSCH
    ST Technical Moderator
    June 22, 2023

    So far you haven't shown any code. How are the following registers configured:

    • CCR
    • PD_DDR
    • PD_CR1
    • PD_CR2
    • EXTI_CR1
    • PWR_CSR

     

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    SRAM.11Author
    Associate III
    June 22, 2023
    #include "stm8s.h"
    #include "stm8s_clk.h"
    #include "stm8s_adc1.h"
    #include "stm8s_gpio.h"
    #include "stm8s_tim2.h"
    #include "main.h"
    #include "flash.h"
    //#include "stm8s_iwdg.h"
    //#include "stm8s_awu.h"
    #include "stm8s_exti.h"
    
    
    
    
    volatile unsigned short _500ms_tick;
    volatile unsigned short idle_counter;
    
    void Clk_Config(void);
    void ADC_Config(void);
    void GPIO_Config(void);
    void EXTI_Setup(void);
    void ADC_Read1(uint16_t *MV);
    void ADC_Read2(uint16_t *Vbat);
    void ADC_Read3(uint16_t *Ocd);
    void ADC_Read4(uint16_t *Temp) ;
    	void AWU_Config(void);
    main()
    {
    uint16_t MV=0,Vbat=0,Ocd=0,Temp=0;
    	unsigned short i;
    	int counting = 0;
    
    
    	Clk_Config();
    	
    	ADC_Config();
    	
    	GPIO_Config(); 
    		
    
    	EXTI_Setup();
    
    	
    	while(MV<100)
    	{
    		ADC_Read1(&MV);
    	 delay_ms(100);
    		Set_LED(0);
    		idle_counter++;
    		
    		if (idle_counter>=300)
    		{
    		
    		 EnterSleepMode();
    		}
     
    	}
    	
    	 
    	
    	while (1)
    	
    	{
    	ADC_Read1(&MV);
     delay_ms(100);
    		
    	ADC_Read2(&Vbat);
    	delay_ms(100);
    	
    	ADC_Read3(&Ocd);
    		delay_ms(100);
    		
    	ADC_Read4(&Temp);
     delay_ms(100);
    	
     if (MV > 20) // Mains Detect
     //WakeupFromSleep();
    		{
     if ((MV < 370) && (Vbat > 227)) // Mains Fail
    					{
     En_Emergency(1); 
    						Set_LED(0);
    												
    					}
    			 			
     else 
     {
     En_Emergency(0);
    						Set_LED(0);
    			 }
    				
    			 
    				
    		}
    		if(MV<=10)
    		{
    			ADC_Read3(&Ocd);
    			delay_ms(100);
    			Set_LED(0);
    						if(Ocd<93 || Ocd>186)
    						{
    						Set_LED(1); 
    						delay_ms(1000);	
    						Set_LED(0); 
    						delay_ms(1000);	
    						Set_LED(1); 
    						delay_ms(1000);	
    						Set_LED(0); 
    						delay_ms(1000);	
    						Set_LED(1);
    						delay_ms(1000);	
    						Set_LED(0); 				
    				
    							delay_ms(5000);	
    				
    						}
    				else if(Ocd>93 || Ocd<186)
    				{
    				Set_LED(0);
    				}
    			
    	}
    	
    		ADC_Read2(&Vbat);
    			if (MV < 250)
    			{
    				Set_LED(0);
    			}
    			else if(Vbat>460 || Vbat < 155)
    			 {
    					Set_Bch(1);
    					Set_LED(0);
    				}
    			else if( Vbat>395)
    			 {
    					
    					Set_LED(1); 
    					Set_Bch(0);
    				}
    			else if(Vbat<383)
    				{
    						Set_LED(1); 
    						Set_Bch(1);
    				}
    			ADC_Read4(&Temp);
    			if(Temp>87 || Temp>425)
    			{
    				Set_Bch(1);
    			}
    			else //if(Vbat<87 || Vbat>425)
    			{
    			 Set_Bch(0);
    				Set_LED(1); 
    				delay_ms(1000);	
    				Set_LED(0); 
    				delay_ms(1000);	
    				Set_LED(1); 
    				delay_ms(1000);	
    				Set_LED(0); 
    				delay_ms(5000);
    			 
    			}
    			
    			
    
    			
    			
    
    
    }
    }
    
    
    
    void Clk_Config() // INTERNAL CLOCK CONFIGUARATION
    	{
    	CLK_DeInit();
    	
    	CLK_HSECmd(DISABLE);
    	CLK_LSICmd(DISABLE);
    	CLK_HSICmd(ENABLE);
    	while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);
    	
    	CLK_ClockSwitchCmd(ENABLE);
    	CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV2);
    	CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
    	
    	CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, 
    	DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
    	
    
    	CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, ENABLE);
    	 CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE);
    	}
    
    void ADC_Config() // ADC INITIALIZATION
    	{
    		 ADC1_DeInit();
    		
    		 ADC1_Cmd(ENABLE);
    
     ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);
    		
    	}
    	
    void ADC_Read1(uint16_t *MV)
    {
    	
    	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, // MAINS INPUT
    					 ADC1_CHANNEL_5,
    					 ADC1_PRESSEL_FCPU_D2, 
    					 ADC1_EXTTRIG_GPIO, 
    					 DISABLE, 
    					 ADC1_ALIGN_RIGHT, 
    					 ADC1_SCHMITTTRIG_CHANNEL5, 
    					 DISABLE);
     ADC1_StartConversion();
     while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
     {
     // Wait for conversion to complete
     }
    
     *MV= ADC1_GetConversionValue();
    
    }
    void ADC_Read2(uint16_t *Vbat)
    {
    	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, //ADC Channel_4 VBATT
    					 ADC1_CHANNEL_4,
    					 ADC1_PRESSEL_FCPU_D2, 
    					 ADC1_EXTTRIG_GPIO, 
    					 DISABLE, 
    					 ADC1_ALIGN_RIGHT, 
    					 ADC1_SCHMITTTRIG_CHANNEL4, 
    					 DISABLE);
     ADC1_StartConversion();
     while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
     {
     // Wait for conversion to complete
     }
    
     
    	*Vbat=ADC1_GetConversionValue();
    }
    void ADC_Read3(uint16_t *Ocd) // ADC Channel_2 OPEN CIRCUIT DETECTION
    {
    	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 
    					 ADC1_CHANNEL_2,
    					 ADC1_PRESSEL_FCPU_D2, 
    					 ADC1_EXTTRIG_GPIO, 
    					 DISABLE, 
    					 ADC1_ALIGN_RIGHT, 
    					 ADC1_SCHMITTTRIG_CHANNEL2, 
    					 DISABLE);
     ADC1_StartConversion();
     while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
     {
     // Wait for conversion to complete
     }
    
     
    	*Ocd=ADC1_GetConversionValue();
    }
    void ADC_Read4(uint16_t *Temp) // ADC Channel_2 TEMPARATURE MONITORING
    {
    	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 
    					 ADC1_CHANNEL_3,
    					 ADC1_PRESSEL_FCPU_D2, 
    					 ADC1_EXTTRIG_GPIO, 
    					 DISABLE, 
    					 ADC1_ALIGN_RIGHT, 
    					 ADC1_SCHMITTTRIG_CHANNEL3, 
    					 DISABLE);
     ADC1_StartConversion();
     while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
     {
     // Wait for conversion to complete
     }
    
     
    	*Temp=ADC1_GetConversionValue();
    }
    
    void GPIO_Config(void)
    	{
    								//GPIO INPUTS
    			
    		//GPIO_Init(GPIOD,GPIO_PIN_2,GPIO_MODE_IN_FL_NO_IT);			// TEMP SENSE
    		GPIO_Init(GPIOD,GPIO_PIN_3,GPIO_MODE_IN_FL_NO_IT);			//VBATT
    		GPIO_Init(GPIOD,GPIO_PIN_5,GPIO_MODE_IN_FL_NO_IT);			//MAINS INPUT
    		GPIO_Init(GPIOC,GPIO_PIN_4,GPIO_MODE_IN_FL_NO_IT);			// OCD SENSE
    		
    		
    								//GPIO OUTPUTS
    								
    		GPIO_Init(GPIOA,GPIO_PIN_3,GPIO_MODE_OUT_PP_LOW_FAST);			// MAIN LAMP
    		GPIO_Init(GPIOC,GPIO_PIN_3,GPIO_MODE_OUT_PP_HIGH_FAST);			//LED O/P
    		GPIO_Init(GPIOC,GPIO_PIN_5,GPIO_MODE_OUT_PP_LOW_FAST);			//BCH
    		
    	}
    void TIM2_Config(void)
    {
     TIM2_TimeBaseInit(TIM2_PRESCALER_32768, 244);
     TIM2_ClearFlag(TIM2_FLAG_UPDATE);
     TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);
     TIM2_Cmd(ENABLE);
    		AWU_DeInit();
    		
    		/* auto wake up at 32ms */
    		AWU_Init(AWU_TIMEBASE_32MS);
    		
    		/* enable auto wake up*/
    		AWU_Cmd(ENABLE);
    		
    		enableInterrupts();
    }
    
    
     
    INTERRUPT_HANDLER(TIM2_UPD_OVF_BRK_IRQHandler, 13)
    {
     if (TIM2_GetITStatus(TIM2_IT_UPDATE) != RESET)
     {
    			
     // Increment the idle_counter every 500ms
     idle_counter++;
    
     // Enter sleep mode if idle for approximately 30 seconds (60 * 500ms)
     if (idle_counter >= 300)
     {
     EnterSleepMode();
     }
    				TIM2_ClearITPendingBit(TIM2_IT_UPDATE);
     }
    }
    
    void EnterSleepMode(void)
    {
     // Disable TIM2 interrupt
     TIM2_ITConfig(TIM2_IT_UPDATE, DISABLE);
    
     // Disable ADC peripheral
     ADC1_Cmd(DISABLE);
    
     // Disable GPIO inputs
     GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_IN_PU_NO_IT);
     GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_IN_FL_IT);
     GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_PU_NO_IT);
    
     halt();
    
     // Re-enable ADC peripheral
     
    }
    
    void Inc500mSCounter(void)
    {
     if (_500ms_tick < 500)
     {
     _500ms_tick++;
     }
     else
     {
     _500ms_tick = 0;
     idle_counter++;
     }
    }
    /*void IWDG_Config(void)
    	{
    		uint8_t WTG_TIME;
    	
    		IWDG_Enable();
    		
    	
    		IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);
    		
    		
    		IWDG_SetPrescaler(IWDG_Prescaler_128);
    		
    		
    		IWDG_SetReload( WTG_TIME);
    		
    		
    		IWDG_ReloadCounter();
    		
    	}*/
    /*void AWU_Config(void)
    {
    	AWU_Init(AWU_TIMEBASE_32MS);
    		
    	
    		AWU_Cmd(ENABLE);
    		
    		enableInterrupts();
    }*/
    
    
    
    
    void EXTI_Setup(void)
    {
    	EXTI_DeInit();
    	EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOD, EXTI_SENSITIVITY_RISE_ONLY);
    	EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_RISE_ONLY);
    
    }
    
    void WakeupFromSleep(void)
    {
    	ADC1_Cmd(ENABLE);
    
     // Re-enable GPIO inputs
     GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_IN_FL_NO_IT);
     GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_IN_FL_NO_IT);
     GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT);
    
     // Reset idle counter
     idle_counter = 0;
    
     // Re-enable TIM2 interrupt
     TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);
     
    }
    INTERRUPT_HANDLER(EXTI_PORTD_IRQHandler, 6)
    {
    	 //EXTI_ClearITPendingBit(EXTI_PORT_GPIOD);
     { // Wake up from sleep mode
     WakeupFromSleep();
     }
    }
    
    
    
    

    for this code my sleep function is working if i enable Apologies for any confusion in this code as I am literally working on it to sort it out .I am in an independent work environment no teams to help it out.Little struggle in developing the code