Skip to main content
llebotlan
Associate II
Jan 12, 2006 12:21 PM UTC
Question

wakeup detection level in LPWFI mode

Posted on January 12, 2006 at 13:21

wakeup detection level in LPWFI mode

This topic has been closed for replies.

4 replies

llebotlan
llebotlanAuthor
Associate II
Jan 12, 2006 4:18 AM UTC
Posted on January 12, 2006 at 05:18

Hello,

I have problems to wake up my str710 when I am in LPWFI mode on the RTC. I am waiting a FallingEdge on the XTI15.

Is there a minimum time for the str to notice the edge.

Thanks,

Ludo

tech9
Associate III
Jan 12, 2006 11:09 AM UTC
Posted on January 12, 2006 at 12:09

Hi Ludo,

here is a sample of my code; it might help you.

//Configure external interrupt

XTI_Init(); //initialize the XTI

XTI_LineModeConfig(XTI_Line15, XTI_FallingEdge); //Configure the line 15 mode ,select Falling edge trig

XTI_LineConfig(XTI_Line15, ENABLE); //Enable line 15 WAKEUP pin or RTC Alarm

You basically need to enable the external interrupts and mostly, enable the RTC alarm to be recognised as such, so it effectively wakes up the MCU. Consult the XTI section of the manual to see more capabilities from this module.

Hope this helps!

Regards,

Jp

llebotlan
llebotlanAuthor
Associate II
Jan 12, 2006 12:01 PM UTC
Posted on January 12, 2006 at 13:01

Sorry, in fact my question was not clear.

My problem is not only to wake up the str but to detect short fallingedge.

Example : a strobe.

What is the minimum strobe length, the mcu can detect ?

Thank you,

Ludo

llebotlan
llebotlanAuthor
Associate II
Jan 12, 2006 12:21 PM UTC
Posted on January 12, 2006 at 13:21

Sorry, in fact my question was not clear.

My problem is not only to wake up the str but to detect short fallingedge.

Example : a strobe.

What is the minimum strobe length, the mcu can detect ?

Thank you,

Ludo