Skip to main content
mymail2000
Associate
Jul 7, 2005 5:22 AM UTC
Question

Vstby value

Posted on July 07, 2005 at 07:22

Vstby value

This topic has been closed for replies.

2 replies

mymail2000
Associate
Jul 7, 2005 4:54 AM UTC
Posted on July 07, 2005 at 06:54

Hi

According to the datasheet, the lowest stand-by voltage Vstby = 4.0V (without RTC and 32kHz oscillator).

On the final version of ST10F276, could the Vstby be lower than 4V?

Thanks

najoua
Associate
Jul 7, 2005 5:22 AM UTC
Posted on July 07, 2005 at 07:22

Hi,

No the Vstby could not have a value lower than 4V. I think you ask this because you want to use a battery to back up the device in standby mode and that the batteries are usually 3.3V but unfortunatly this is not possible.

Regards,