Skip to main content
JMI
Associate
January 7, 2020
Question

VNQ5E160AK 1) current sense limits 2) internal power limitation

Hi, I'm using some VNQ5E160AK with current monitoring. According to datasheet Iout/Isense ratio is in the range of 465 for 'high' current, means it should be 6.5mA for 3A and 21.5mA for 10A. As my ADC range is 5V, I load sense pin with a 200 Ohm resistor (=> 4.3V full load).

This work fine at 2.5A (~5mA sense), but don't work anymore with a load at 4A. I believe it's related to Isensh.

To detect power limitation (over load), datasheet tell to charge sense pin with a 3.9KOhm resistor to get 8V, which look strange for me as this imply ~2mA sense and 0.95A load...

Not funny: I use for test a 12V 10A power supply, when I 'overload' output at 8.3A (a 100W bulb), driver burn instantaneously, it even don't try to limit power for overheating (thermal copper area is more than 4cm^2)

Thanks for your help, regards

This topic has been closed for replies.

1 reply

JMI
JMIAuthor
Associate
January 8, 2020

Well, find answer my self reading UM1556: Isense is internally limited to about 11mA by M1, so "no way" to get 21.5mA for 10A. In fact, if you assume a K factor of 465, you won't be able to monitor a current higher than 5.1A ! doesn't matter what you put for resistor load. (it's even worst as K factor decrease with Io).

If you consider case of overtemp, Sense pin becomes a voltage source limited to 8mA, if you want to make difference between 'normal' operation and others, you have to consider 8mA is maximum for normal operation, which (with this 465 K factor) give you a 3.7A load !

So, if you plan to use Isense with Vpower5 devices, you need to choose a 10A HSD to drive 3.5A... and this is true for VNQ5E160AK, VND5E160AJ etc

Other one I use is VN5050AJ, this one has a K factor of 1970 and so: work well up to 15A.

I had a quick look on Vpower7 serie, looks like they have the same K factor range and even lower Isense limitation!

Finally, I believe there is no real limitation on M1 Mos, that could be the reason driver burn when I load it with 8.3A, no related to main but to sense circuit.