Skip to main content
lucio
Associate
Jan 11, 2005 6:49 PM UTC
Question

VGA-LCD

Posted on January 11, 2005 at 19:49

VGA-LCD

This topic has been closed for replies.

2 replies

lucio
lucioAuthor
Associate
May 11, 2004 9:10 AM UTC
Posted on May 11, 2004 at 11:10

Hi,

I'm using an STPC Consumer with a TFT 1024x768 LCD connected

to the on board VGA. I'm using the VGA BIOS from Elpin System.

The problem was that work at a frequency of 63Hz instead a

frequency of 60Hz. I'm not familiar with the VGA register, can you

help me to focus on the register intrested on frequency adjust

and screen centering

thanks
uwe
Visitor II
Jan 11, 2005 6:49 PM UTC
Posted on January 11, 2005 at 19:49

Do you have a VGA register set example for a 1024x768 display ?

Perhaps in a 32kBios, even with 63 Hz.

Best Regards

Flipflop