Skip to main content
SWiel.1
Associate
September 21, 2020
Solved

Using SWIM from STM8S Discoveryboard for STM8AF

Hello community,

after unsoldering the solderbridges of the STM8S-Disco-Board, I try to connect the SWIM to a STM8AF Chip. I read in the manueal, that this is not possible (only for STM8S-Family). But after trying it, I could flas Code on the µC and Debug it with the STVD. For example, a counter in my programm ist counting up :)

But if I want to switch Timer1-Output-Pin from LOW to HIGH, nothing happens.

Is ist possible,, that I can program the µC and it is running without errors, but the mapping of the GPIOs are not correctly done?

Is there a influence of the SWIM-adapter even if I had chosen the STM8AF-Chip in STVD?

Thank you all, Steffen

    This topic has been closed for replies.
    SWiel.1
    SWiel.1Best answer
    Associate
    September 25, 2020

    Hello Ozone, hello Community,

    I'm sorry, but the problem was on my side:

    Our PCB has some defect connections, that was the reason why I could not switch the TIM1 Pin. When I now switch an unconnected pin, I can regulate the output via Software.

    So, despite of the hint in the UM 8017 we can use the STM8S-Discoboard SWIM to connect STM8AF µCs ;)

    Nevertheless, today I received my ST-LINK-V2 device, so I do not use the discoboard for those purpose anymore.

    3 replies

    Ozone
    Principal
    September 21, 2020

    I suppose the firmware of the STM8S SWIM controller on the STM8S-Disco is limited to the S family, most probably because of code/Flash size reasons.

    Thus, you are likely running an incorrect configuration.

    Perhaps you can "update" the SWIM firmware to that of a STM8AF device.

    Had been severeal years since I had been working with STM8s, though.

    SWiel.1
    SWiel.1Author
    Associate
    September 21, 2020

    Hi Ozone,

    Thank you very much for the quick answer :)

    This is exactly what I'm afraid of. (the incorrect configuration).

    Does anyone know, where I can find an "update" from STM8S to STM8AF? On the ST hompage I did not found anything - only updates of the SWIM itself, bur not for different µCs

    SWiel.1
    SWiel.1AuthorBest answer
    Associate
    September 25, 2020

    Hello Ozone, hello Community,

    I'm sorry, but the problem was on my side:

    Our PCB has some defect connections, that was the reason why I could not switch the TIM1 Pin. When I now switch an unconnected pin, I can regulate the output via Software.

    So, despite of the hint in the UM 8017 we can use the STM8S-Discoboard SWIM to connect STM8AF µCs ;)

    Nevertheless, today I received my ST-LINK-V2 device, so I do not use the discoboard for those purpose anymore.