Skip to main content
rfsingh81
Associate
Aug 29, 2014 2:00 PM UTC
Question

Using COSMIC C - trying to understand Clock setting

Posted on August 29, 2014 at 16:00

Hello there, I am playing with my STM8s Discovery board but unable to set the clock properly. Can someone please put some light on what I am doing wrong. My code is as follows:

---------------------------------------------

&sharpinclude ''stm8s.h''

u16 c=9000;

main()

{

void CLK_Deinit();

void CLK_HSICmd(ENABLE);

void CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV8);

void CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV128);

CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO,CLK_SOURCE_HSI,ENABLE,CLK_CURRENTCLOCKSTATE_DISABLE);

GPIO_DeInit (GPIOD);

GPIO_Init (GPIOD,GPIO_PIN_0,GPIO_MODE_OUT_PP_LOW_FAST);

// TIM2_DeInit();

// TIM2_TimeBaseInit(TIM2_PRESCALER_2048, 300);

// TIM2_Cmd(ENABLE);

while (1){

/* if (TIM2_GetCounter()>150){

GPIO_WriteHigh(GPIOD,GPIO_PIN_0);

}

else {

GPIO_WriteLow(GPIOD,GPIO_PIN_0);

}*/

while (c>1){

c--;

}

GPIO_WriteReverse(GPIOD,GPIO_PIN_0);

c=9000;

}

}

-----------------------------------

My LED blinks at the same rate even when I change the HSI prescaler and/or sys clock config. Thanks

#stm8s-clock-setting
    This topic has been closed for replies.