Skip to main content
pub
Visitor II
Aug 11, 2011 11:06 PM UTC
Question

use rs232 uart with stm8l discovery board

Posted on August 12, 2011 at 01:06

Hi,

I would like to use the uart device of the stm8l chip on the stm8l discovery board.

I notice that uart and cristal are shared on the same pins (PA2 and PA3)

Do you think it is possible to use the uart when the stm8l is working with the 32khz oscillator or on the internal 16 Mhz internal RC ?

I don't care of the speed RS232 speed, even 300 bauds is fine for me,

Thanks,

Franck

    This topic has been closed for replies.

    1 reply

    bomber123433307
    Visitor II
    May 14, 2013 7:47 PM UTC
    Posted on May 14, 2013 at 21:47

    Hi Just use alternate function on other pins. you can get the alternate function pins from the stm8l's datasheet.