Skip to main content
tom7
Associate III
Sep 22, 2004 8:30 AM UTC
Question

use P6.2 as discrete I/O on ST10F276

Posted on September 22, 2004 at 10:30

use P6.2 as discrete I/O on ST10F276

This topic has been closed for replies.

2 replies

tom7
tom7Author
Associate III
Sep 22, 2004 8:07 AM UTC
Posted on September 22, 2004 at 10:07

I have to use P6.2 as discrete I/O.

The bus interface is configured for using two CS-signals therefore the

P6.2 port pin should be available.

Register RP0H is 0x00e2, so bus-cfg should be ok.

When I try to access the pin, my system crashes.

I looked at the disassembled opcode with my debugger how I'm accessing the

pin :

OR P6,#0x04

OR DP6,#0x04

AND P6,0xfffb <- here it crashes.

I'm using Tasking v8.0 with xview rom-monitor debugger via ASC0 interface.

Does someone has an idea what's going on there ?

tom.

tom7
tom7Author
Associate III
Sep 22, 2004 8:30 AM UTC
Posted on September 22, 2004 at 10:30

Problem sorted out, it was a board ''feature'' .