Skip to main content
gordon239955
Visitor II
November 15, 2021
Question

USBLC6-4SC6 for EFT and lightning protection

Hi,

Can USBLC6-4SC6 be used to protect an IO from EFT (IEC 61000-4-4) and lightning (IEC 61000-4-5)? I do not see any specification for these standards? Thanks.

Regards

Gordon

This topic has been closed for replies.

1 reply

FGUIT
ST Employee
November 18, 2021

Hi,

Regarding IEC 61000-4-5, USBLC6-4SC6 is able to withstand 5A with a 8/20 µs surge, this is specified on the Table 2.

Best regards.

Fabrice.