Skip to main content
jmartin9
Associate III
Jun 14, 2006 6:22 AM UTC
Question

usb-mouse-demo

Posted on June 14, 2006 at 08:22

usb-mouse-demo

This topic has been closed for replies.

5 replies

jmartin9
jmartin9Author
Associate III
Jun 8, 2006 11:26 AM UTC
Posted on June 08, 2006 at 13:26

hi!

i download the file you can see in attachments, and i would like to know is it works with STR7 RVDK Realview debugger 1.7?

when i tried to buil the project i had errors. Can you help me??

thanks!!

________________

Attachments :

1075381110.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtIH&d=%2Fa%2F0X0000000aLA%2FLPiPaMzlluSNGmODpPKvjuF9zJXCADC8ALYlMK8I4NQ&asPdf=false
jmartin9
jmartin9Author
Associate III
Jun 9, 2006 9:50 AM UTC
Posted on June 09, 2006 at 11:50

hi!!

i had add the line: PRESERVE8. but i had the same problem, when i tried to build the project, i had an error that say:

9 files missing.

can you help me??

thanks

jmartin9
jmartin9Author
Associate III
Jun 12, 2006 10:50 AM UTC
Posted on June 12, 2006 at 12:50

Hi Zouhair!!!

thanks for your the projects works!!!!

i would like ton know where the programm is loaded? they seemed to be loaded in RAM but in the scatter file they seemed to be loaded in FLASH.

can you say me where is loaded???

thanks,

jmartin9
jmartin9Author
Associate III
Jun 13, 2006 6:07 AM UTC
Posted on June 13, 2006 at 08:07

Hi Zouhair,

when you say me to remap RAM to adress 0x00 by hardware, does it mean with switch 15,14,13??

And can you explain me why in the scat file there is specified that the programm is loaded in flash??

you can find in attachments the scat file.

Thanhs,

jmartin9
jmartin9Author
Associate III
Jun 14, 2006 6:22 AM UTC
Posted on June 14, 2006 at 08:22

Hi Zouhair,

Thanks for answer.

-Can you say me if it is possible to run this programm with WinIDEA?

- there is files to replaced?

Thanks,