Skip to main content
Associate
August 6, 2023
Solved

USB issue with STM32F411

This has nothing to do with EEPROM devices, but that was the only "labeI" that would work. I built a custom board using an STM32F411RET6. It has a 12MHz external clock. I'm trying to use a VCP USB interface. The USB code enumerates fine on a 'F407 DISCO board (STM3240G-EVAL), of course with the 25MHz crystal instead of my 12MHz oscillator. But I get the attached USB connection error with my custom board. This interface won't allow me to attach a .zip of my code, and only 3 attachments are allowed, but I can send the CubeMX file I am using, and the actual code.

 

This topic has been closed for replies.
marcmignBest answer
Associate
August 8, 2023

It turned out that the LDO I was using to generate 3.3V from the USB VBUS was only outputing 2V. I changed the feedback resistors on the LDO to give 3.3V, and it started working.

2 replies

TDK
August 7, 2023

Your clock setup and schematic look fine. I would expect it to be a code issue.

Debug your code, ensure all the USB functions are passing correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."
marcmignAuthorBest answer
Associate
August 8, 2023

It turned out that the LDO I was using to generate 3.3V from the USB VBUS was only outputing 2V. I changed the feedback resistors on the LDO to give 3.3V, and it started working.