Skip to main content
daniel52079
Associate II
May 17, 2004 2:45 PM UTC
Question

Usb-example!!

Posted on May 17, 2004 at 16:45

Usb-example!!

This topic has been closed for replies.

2 replies

daniel52079
Associate II
May 17, 2011 10:00 AM UTC
Posted on May 17, 2011 at 12:00

Hi!

I don't know if anybody have tried to compile the uPSD DK3200 USB-example! because it isn't possible to compile! to much source code for the supported DevKit DemoVersion of Keil C-Compiler! What about people which do not have a full version! Must i buy one???

or are there other possibilities!

Best regards

DANIEL

[ This message was edited by: daniel24 on 17-05-2004 16:15 ]
joseph2399
Associate II
May 17, 2011 10:00 AM UTC
Posted on May 17, 2011 at 12:00

The latest released (April 2004) version of the USB demo code is available at:

http://www.st.com/stonline/products/families/memories/psm/soft_c2.htm

It compiles to around 5.5K bytes. The zip file containing the demo code also includes the compiled image in a hex file. Using PSDsoft Express and FlashLink (included in the DK3200 kit), you can load the demo program (hex file) into the memory on the 32xx device on your DK3200 board and try it.

[ This message was edited by: uPSD on 17-05-2004 20:16 ]