Skip to main content
shermantec
Associate III
Dec 1, 2005 9:37 AM UTC
Question

USB End Potins

Posted on December 01, 2005 at 10:37

USB End Potins

This topic has been closed for replies.

2 replies

shermantec
Associate III
Nov 30, 2005 10:51 AM UTC
Posted on November 30, 2005 at 11:51

Hello

We need the address of the end point transmit and receive addresses

The found the following:

ENDP0_RXADDR address (0x80)

ENDP0_TXADDR address (0x90)

ENDP1_TXADDR address (0xA0)

What about the rest of the endpoints address

Thx

Sherman Amir

mohamed23
Associate
Dec 1, 2005 9:37 AM UTC
Posted on December 01, 2005 at 10:37

Hi Latino,

For more details refer to the STR71x Reference manual, USB section or to the USB software user manual.

The small piece of code that u have written is just a demonstration

using the Hid Mouse demo that uses only two physical endpoints :

Endpoint 0 ( Transmission/Reception)

Endpoint 1 ( Transmission)

With regards, :p :-]