Skip to main content
sjo
Associate III
May 16, 2006 11:21 AM UTC
Question

usb control read

Posted on May 16, 2006 at 13:21

usb control read

This topic has been closed for replies.

9 replies

sjo
sjoAuthor
Associate III
Jul 25, 2005 4:58 AM UTC
Posted on July 25, 2005 at 06:58

I have written a dfu driver for the str711 device, all works ok except control read transfers (OUT transfers).

I have traced the problem down to the usb interrupt routine (CTR_ISR) - This function below checks for a setup packet but the mask will also catch all RX (OUT) transfers including non SETUP ones. In other words the Out0_Process will never get called.

if((wEPVal & (EP_CTR_RX|EP_SETUP)) != 0)

{

_ClearEP_CTR_RX(ENDP0); /* SETUP bit kept frozen while CTR_RX = 1 */

Setup0_Process();

}

else if((wEPVal & EP_CTR_RX) != 0)

{

_ClearEP_CTR_RX(ENDP0);

Out0_Process();

}

changing to

if((wEPVal & (EP_SETUP)) != 0) fixes the problem, is this correct ?

Regards

sjo

sjo
sjoAuthor
Associate III
Jul 27, 2005 11:50 AM UTC
Posted on July 27, 2005 at 13:50

Could anyone confirm what I have done is correct ?

Regards

sjo

hichem2
Associate
Jul 28, 2005 5:01 AM UTC
Posted on July 28, 2005 at 07:01

Hi Sjo,

Sorry for the delay...

We have already checked the USB software libray and some mistakes are alredy verified(The new version is not published yet).

Concerning the Out0_Process section we use the following condition .

if((wEPVal &EP_SETUP) != 0)

{

_ClearEP_CTR_RX(ENDP0); /* SETUP bit kept frozen while CTR_RX = 1 */

Setup0_Process();

}

else if((wEPVal & EP_CTR_RX) != 0)

{

_ClearEP_CTR_RX(ENDP0);

Out0_Process();

}

With best regards,

Hich :o

[ This message was edited by: Hich on 28-07-2005 12:45 ]

cgrun
Associate II
Sep 22, 2005 2:38 PM UTC
Posted on September 22, 2005 at 16:38

You inform us that you have a new version of the usb library.

Could you publish it ? even if it's unsupported, because we use the current library that have some problem...

Sincerely

Chris.

cgrun
Associate II
Oct 2, 2005 3:23 PM UTC
Posted on October 02, 2005 at 17:23

Can you puublish this new version of the usb library ?

cgrun
Associate II
Feb 9, 2006 4:54 AM UTC
Posted on February 09, 2006 at 05:54

Did have you any news for the usb lib?

Regards

Chris.

hichem2
Associate
Feb 9, 2006 6:16 AM UTC
Posted on February 09, 2006 at 07:16

Hi all,

The STR71x USB software package review is on going and planned for W13.

Then it will be published as soon as possible.

Thank you for your comprehension.

With best regards,

Hich ;)

shangdawei1
Associate III
Feb 23, 2006 7:43 AM UTC
Posted on February 23, 2006 at 08:43

Quote:

On 09-02-2006 at 11:46, Anonymous wrote:

Hi all,

The STR71x USB software package review is on going and planned for W13.

Then it will be published as soon as possible.

Thank you for your comprehension.

With best regards,

Hich ;)

will it be published before April 1 ?

cgrun
Associate II
May 16, 2006 11:21 AM UTC
Posted on May 16, 2006 at 13:21

Did have you any news for the usb lib (We are in week 20)?

Regards

Chris.