Skip to main content
hariharan2
Associate
Jan 7, 2005 5:42 AM UTC
Question

USB code for uPSD3254A needed - Urgent

Posted on January 07, 2005 at 06:42

USB code for uPSD3254A needed - Urgent

This topic has been closed for replies.

1 reply

hariharan2
Associate
May 17, 2011 10:05 AM UTC
Posted on May 17, 2011 at 12:05

Hi all,

I have a problem in USB. I am using uPSD3254A device and I tried the sample demo application for USB (with windows application) from the STMicroElectronics site. After powering up the board, when I say connect from the windows application (given by ST) it says ''Failed to connect to ST demo board''. Can you provide me the USB code that is running on the uPSD3254A device. Or should I do any modification onto the demo code before downloading into the chip.

Please help me to solve this problem.

Thanks & Regards,

Hariharan