Skip to main content
paulbrown9
Associate III
Jan 17, 2006 3:00 AM UTC
Question

USB Bulk transfer.

Posted on January 17, 2006 at 04:00

USB Bulk transfer.

This topic has been closed for replies.

17 replies

reg007
Associate II
Jan 3, 2006 8:19 AM UTC
Posted on January 03, 2006 at 09:19

hmmm.

I think this is my Problem too.

Has anyone a solution?

regards

anil23
Associate III
Jan 3, 2006 10:46 AM UTC
Posted on January 03, 2006 at 11:46

Nops...not moved any further...

reg007
Associate II
Jan 11, 2006 5:23 AM UTC
Posted on January 11, 2006 at 06:23

damn..... :-Y

I solved my Problem.

There was a bug in the Windows XP (SP1) USB Module.

I patched it, an everything works fine. :o

Be sure to have

http://www.microsoft.com/downloads/details.aspx?FamilyID=733dd867-56a0-4956-b7fe-e85b688b7f86&displaylang=de

installed if your working on WinXp with SP1.

regards

gajeronline
Associate II
Jan 11, 2006 10:16 AM UTC
Posted on January 11, 2006 at 11:16

Hi Guys.

I downloaded bulkusb-ddk.zip, and I have a question, where I can find SDK for this source.

I try compile this source in borland c++, but compilation faild, becouse t i don't have devioctl.h setupapi.h usbdi.h.

anil23
Associate III
Jan 11, 2006 10:22 AM UTC
Posted on January 11, 2006 at 11:22

Hey re-G,

Thanks for the update. I'm on a Win XP SP2 machine. I believe that this update wouldn’t work for me. Can you please forward me the example source code of the bulk transfer.

Regards,

mohamed23
Associate
Jan 16, 2006 2:00 PM UTC
Posted on January 16, 2006 at 15:00

Hi All,

Jungo has a solution named WinDriver that allows one to access a USB device and so send or receive data on pipes directly from User mode.

So you can develop your STR71x USB firmware ( Control/Interrupt/ Bulk/ isochronous) and test it with this Software PC solution in all Windows platforms.

have a look to www.jungo.com

Rgds

:o :o :o

reg007
Associate II
Jan 17, 2006 3:00 AM UTC
Posted on January 17, 2006 at 04:00

Thx Rave.

I'm working with the USB Dev Driver, developed by

http://www.thesycon.com

.

It seems like beeing the same as jungo provides.

But thx for the link.

@ianmali

This is only a bug of SP1. I don't think this patch will work on SP2, sry.

regards