Skip to main content
yangdawei2
Associate
Jun 9, 2010 1:59 AM UTC
Question

USB bulk in interrupt missing

Posted on June 09, 2010 at 03:59

Hi all,

I am debugging a device which connects to PC through USB cable. On PC side, this USB device has been enumerated as a serial port. It works now,  I can see the new COM4 has appeared.

The problem is through the Hyperterminal, I can send many key strokes to device, but there is no data been sent back.

I am using end point1 to transmit, end point 3 to receive data. Through the JTAG, I can see the end point 1's transmission byte counter been set to 1, 1 byte data been write to PMA end point 1's transmission address, end point 1 register's STAT TX[1:0] been set to '11' which means valid. The code is:

u32 VCOM_Send(BYTE* buf, u32 len)

{

    if(len > USBCOMMS_PORT_DATA_SIZE)

    {

        remainData = len - USBCOMMS_PORT_DATA_SIZE;

        len = USBCOMMS_PORT_DATA_SIZE;

    }

   

    UserToPMABufferCopy(buf, ENDP1_TXADDR, len);

    SetEPTxCount(ENDP1, len);

    SetEPTxValid(ENDP1);

    return 0;

}

But there is no interrupt happens after the VCOM_Send(). At the same time, the bit DTOG_TX and bit CTR TX in end point 1 register are all cleared which should be set by hardware.

The end point descriptor is:

    /*Endpoint 3 Descriptor*/

    0x07,  /* bLength: Endpoint Descriptor size */

    USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: Endpoint */

    0x03, /* bEndpointAddress: (OUT3) */

    0x02, /* bmAttributes: Bulk */

    USBCOMMS_PORT_DATA_SIZE,  /* wMaxPacketSize: */

    0x00,

    0x00,  /* bInterval: ignore for Bulk transfer */

    /*Endpoint 1 Descriptor*/

    0x07,  /* bLength: Endpoint Descriptor size */

    USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: Endpoint */

    0x81, /* bEndpointAddress: (IN1) */

    0x02, /* bmAttributes: Bulk */

    USBCOMMS_PORT_DATA_SIZE,  /* wMaxPacketSize: */

    0x00,

    0x00  /* bInterval: ignore for Bulk transfer */

Is there any one can give any clues that I can go further to find the problem?

Thanks in advance!

Dawei

This topic has been closed for replies.

2 replies

tsuneo
Associate II
Jun 11, 2010 2:16 PM UTC
Posted on June 11, 2010 at 16:16

1) Is the bulk IN endpoint enabled and initialized in _Reset() callback?

(ST USB stack does it in bus reset handler, but better USB coding practice is doing it in Set_Configuration handler)

2) Do you have an interrupt IN endpoint on the Communications Class interface?

Also, is this endpoint is enabled / initialized ?

Even if you don't send any Serial_State notification over the interrupt IN endpoint, this endpoint is required.

Without this endpoint, Windows CDC driver (usbser.sys) stops polling on the bulk IN endpoint, too.

Tsuneo

yangdawei2
Associate
Jun 15, 2010 12:42 AM UTC
Posted on June 15, 2010 at 02:42

Hi Tsuneo,

Thank you for your reply.

This problem has been fixed by some changes in the end point settings. I could not make sure what is the exact change, but it works after I reconfigured the sending and reveiving addresses of end point 0, 1 and 3.

Cheers,

Dawei