Skip to main content
tong
Associate III
Apr 24, 2004 7:43 PM UTC
Question

uPSD3212 Memory Mapping Help

Posted on April 24, 2004 at 21:43

uPSD3212 Memory Mapping Help

This topic has been closed for replies.

2 replies

tong
tongAuthor
Associate III
May 17, 2011 10:00 AM UTC
Posted on May 17, 2011 at 12:00

Hi

I am using the uPSD3212, and planning to have the primary flash as program space and the secondary as the data space.

The primary flash is devided in to 4 sector of 16K and I am planning to stack them up from 0x0000 to 0xFFFF.

The socondary flash is 16K and I am planning to have it as two banks of 8K each and

Please tell me if this will work ok or not?

tong
tongAuthor
Associate III
May 17, 2011 10:00 AM UTC
Posted on May 17, 2011 at 12:00

Thank You

Maybe I will ask you some more question when I do this.

Since you have done it. If you don't mind.

Thanks again.