Skip to main content
mikebartholomew9
Associate
Sep 24, 2004 12:33 AM UTC
Question

uPSD Sound Studio and uPSD32xx/uPSD33xx Setup

Posted on September 24, 2004 at 02:33

uPSD Sound Studio and uPSD32xx/uPSD33xx Setup

This topic has been closed for replies.

2 replies

joseph2399
Associate II
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

Please send your questions to the application engineering department at:

mailto:apps.psd@st.com

. Also provide the following information so we can better help you:

Name

Company Name

Phone Number

Location (City, State, Country)

Production uPSD part number (3234, 3334, etc.)

Application

Projected annual volume (units)

Production start date

Thanks,

uPSD Applications Engineering

mikebartholomew9
Associate
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

We are interested doing sound generation using uPSD33xx as noted in Application note AN2007.

Question 1: Where do you download the uPSD Sound Studio V1.0 application?

Question 2: The application note example used the 8 pages of main flash memory (fs0-fs7). If we expanded the number of pages using external flash, can the uPSD Sound Studio handle these extra pages when creating the final HEX files for the PSD Soft Express utility?

The uPSD Sound Studio application appears to work only with uncompressed .WAV files. The 256K main flash is limited for our needs but if we add the maximum addressable flash externally we'd have more than enough.