Skip to main content
janek
Associate III
Sep 7, 2005 12:04 PM UTC
Question

uPSD being very slow

Posted on September 07, 2005 at 14:04

uPSD being very slow

This topic has been closed for replies.

2 replies

janek
janekAuthor
Associate III
May 17, 2011 10:08 AM UTC
Posted on May 17, 2011 at 12:08

ST did a good job with flash and PLD around 8051, but it is still the same architecture - very slow and C inefficient.

As an example I have the same C source compiled an run on:

1) 8MHz MSP430 using Crossworks compiler

2) 11.0592MHz uPSD3233B using Keil compiler

The execution time for communication task is:

for MSP430 - 25s

for uPSD3233B -240s

Are there any ways (other than increasing clock speed) to make it run with an reasonable efficiency?

(It is not my project, I am helping someone, who wants to stay with the 8051 micro)

Any suggestions will be appreciated.

joseph2399
Associate II
May 17, 2011 10:08 AM UTC
Posted on May 17, 2011 at 12:08

Have a look at the Turbo Series (uPSD33xx and uPSD34xx). Some architectural enhancements have been made that significantly increase performance over the uPSD32xx products.