Skip to main content
sandeep2
Associate III
Jun 4, 2009 10:20 AM UTC
Question

Unable to set the SCAN bit in ADC_CR2

Posted on June 04, 2009 at 12:20

Unable to set the SCAN bit in ADC_CR2

    This topic has been closed for replies.

    2 replies

    mozra27
    Visitor II
    May 17, 2011 1:03 PM UTC
    Posted on May 17, 2011 at 15:03

    Hi Sandeep,

    The ''Scan mode for single and continuous conversion of a sequence of channels'' feature doesn’t available for the STM8S20xx product if you need this feature you can use STM8S105x product.

    For more details about the products features availability refer to the products datasheet

    Regards

    mozra

    sandeep2
    sandeep2Author
    Associate III
    May 17, 2011 1:03 PM UTC
    Posted on May 17, 2011 at 15:03

    Hi,

    We are using the STM8S 128 eval board, RLink debugger and STVD toolset.

    We are unable to use the ''single scan mode'' of ADC. Setting the SCAN bit of ADC_CR2 doesn't actually set the bit and there is no change in the status.

    We even tried to modify the register value manually using the Peripheral register's view with STVD and also from the Memory view window.

    But it just doesn't let us set the SCAN bit.

    Please let us know if there is any solution for this.

    Regards,

    SU