Skip to main content
Associate
August 30, 2024
Question

Ultra low power consumption with STM8L151K4T6 + RFM90W.

Hi I am starting a project for ultra low power consumption with STM8L151K4T6 + RFM90W, but not getting lora library for RFM90W.

Please help me with library and sample tx and rx code.

It will be very helpful, please suggest.

    This topic has been closed for replies.

    7 replies

    Peter BENSCH
    ST Technical Moderator
    August 30, 2024

    Welcome @SunnyKatiyar09, to the community!

    Have you ever used your favourite search engine to search for "STM32 RFM90W", for example?

    I can immediately find a GitHub repository stm32-hal-rfm95 that you could start with. But remember that if you have any questions, you'll only get support there.

    Good luck!
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Peter BENSCH
    ST Technical Moderator
    August 30, 2024

    Oops, I only realised afterwards that it wasn't about STM32, but STM8, sorry. But I don't hold out much hope that someone has done something there.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Associate
    September 2, 2024

    Hi,

    The purpose to STM8L151K4T6 + RFM90W is,

    it required very low power to operate (1.8V) and this will very helpful for our project.

    Current I have solutions for power supply, and now enhancing our project that work with battery supply for long life.

    If any better solution for this please suggest.

    Tesla DeLorean
    Guru
    August 30, 2024

    That would seem like someone else's project..

    I think CDEBYTE had some STM8 example for their Semtech designs.

    Not sure there's anything magic for the RFM90W you couldn't port from other SX126x libraries or examples

    https://www.hoperf.com/modules/lora/RFM90CW.html

    They have some STM32F103 based code, perhaps start reviewing that, and how it might port.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    MM..1
    Super User
    September 2, 2024

    Maybe show your idea, because module with RX 8mA and TX 100mA is ultra low power as ...

    Associate
    September 5, 2024

    Hi, Thank you for your reply,

    I am working on Wireless Water Level Controller/Monitor (Using atmega328 and lora ra-01),

    Now I am using power supply to Tx, but want to switch to battery for long life.

    I have purchased STM8L151K4T6 and rfm90 (Both are working on low power as per datasheet)

    1. question here : Is it possible to communicate between Rx(Atmega328+Lora ra-01) with Tx(STM8L151K4T6+Lora ra-01)?

    2. Will it help to save battery power ? (with interrupt and deep sleep)

    If yes then please provide some solutions from Tx side (lora library with sample).

    If No, Please suggest.

    Thank you so much.

    Associate
    September 28, 2024

    I have made Receiver as (Atmega328+lora sx1278) and Transmitter as (STM8L151K4T6+lora sx1278), 

    Configured SPI pins and its able to communicate data.

     

    Thank you so much for your suggestion.