Skip to main content
sh_it
Visitor II
Jul 14, 2016 12:09 PM UTC
Question

UART2 of STM8S not working with HSI clock

Posted on July 14, 2016 at 14:09

Hi I am prashant. I am using stm8s microcontroller with uart2 . First thing is that when i am using uart explicitly without configure the clock to 16Mhz ( HSI clock), uart throwing the garbage values. Secondly when i configure the clock to HSI(16Mhz) , program gets blocked to wait for the TXE bit (UART2_FLAG_TXE)  to set forever. It happens only when i configure the system clock to HSI otherwise throw the garbage value.

I am posting my code below.

&sharpinclude ''stm8s_uart2.h''

&sharpinclude ''stm8s_clk.h''

void clk_config()

{

  //CLK_DeInit();

  //CLK_HSICmd(ENABLE);

  CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);

}

void uart_config()

{

  UART2_DeInit();

  UART2_Init(9600, UART2_WORDLENGTH_8D, UART2_STOPBITS_1, UART2_PARITY_NO, UART2_SYNCMODE_CLOCK_DISABLE, UART2_MODE_TXRX_ENABLE);

  UART2_Cmd(ENABLE);

}

int main( void )

{

  //clk_config();

  uart_config();

  while(1)

  {   

    UART2_SendData8('P');    //sending some garbage value rather character 'P' when  HSI clock isn't configured.

    while(UART2_GetFlagStatus(UART2_FLAG_TXE) == RESET);     //program remains blocked here if i uncomment the clock_config()

  }

  return 0;

}

#hsi #stm8s #uart #stm8
This topic has been closed for replies.