Skip to main content
Chayan Roy
Associate III
Nov 9, 2017 10:13 AM UTC
Question

UART1 RECEIVE is not working

Posted on November 09, 2017 at 11:13

Hello,

Actually I am interfacing ESP8266 wifi module with STM8S003F3P6 MCU . I have  programed the wifi module to get data from internet and send it to STM8S003F3P6. Data is character 1 or 0. Wifi module is working wel.But it seems that there is nothing happening from the STM8S003F3P6 Side. Kindly  if anyone can guide me,if I am doing anything wrong. Thanks.

#include 'STM8S003F3P.h'

void InitialiseSystemClock(void);

void UART1_Initialize(void);

    

void UART1_Initialize(void){

UART1_CR1=(0<<4);

UART1_BRR1=0x08;

UART1_BRR2=0X0a;

UART1_CR2=(1<<5);

UART1_CR2=(1<<2);

}

void main(void){

                   InitialiseSystemClock();

    

                                                            

               UART1_Initialize();

      PD_DDR |=(1<<3);

          PD_CR1 |=(1<<3);

          PD_CR2 |=(1<<3);

                                        

                 _asm('rim');

                   

                                 while(1){

                                             

            

                                 }

}

 void InitialiseSystemClock(void)

                         {

                            CLK_ICKR = 0;                       //  Reset the Internal Clock Register.

                               CLK_ICKR = (1<<0);;                 //  Enable the HSI.

                            CLK_ECKR = 0;                       //  Disable the external clock.

                             while (!(CLK_ICKR & (1<<1)));       //  Wait for the HSI to be ready for use.

                               CLK_CKDIVR = 0;                     //  Ensure the clocks are running at full speed.

                               CLK_PCKENR1 = 0xff;                 //  Enable all peripheral clocks.

                                   CLK_PCKENR2 = 0xff;                 //  Ditto.

                                      CLK_CCOR = 0;                       //  Turn off CCO.

                                      CLK_HSITRIMR = 0;                   //  Turn off any HSIU trimming.

                                         CLK_SWIMCCR = 0;                    //  Set SWIM to run at clock / 2.

                                          CLK_SWR = 0xe1;                     //  Use HSI as the clock source.

                                          CLK_SWCR = 0;                       //  Reset the clock switch control register.

                                     CLK_SWCR = (1<<1);                  //  Enable switching.

                                 while (CLK_SWCR & (1<<0));        //  Pause while the clock switch is busy.

                                    }

@far @interrupt void UART1_RECV_INTERRUPT (void){

read=UART1_DR;

if(read =='1'){

PD_ODR |=(1<<3);

}

else{

if(read =='0'){

PD_ODR &=~(1<<3);

}

}

}
    This topic has been closed for replies.