Skip to main content
ongth60
Associate III
June 7, 2005
Question

uart0 example

Posted on June 07, 2005 at 11:24

uart0 example

This topic has been closed for replies.

9 replies

ongth60
ongth60Author
Associate III
June 2, 2005
Posted on June 02, 2005 at 07:56

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6Xf&d=%2Fa%2F0X0000000bqF%2FZGV_ciO95N4jBwH_4CGPA2AufwZt_isVMY06ED06h9s&asPdf=false
yu-jun
Associate
June 2, 2005
Posted on June 03, 2005 at 00:28

I think that you should disable the UART0''s recieve ( UART_RxConfig(UART0, DISABLE); ) before you send data using UART0, after sending data you enabel recieve.

Try it.

weigelt
Associate
June 3, 2005
Posted on June 03, 2005 at 05:42

Hello Ongth,

First thing, the following line in your posted code is wrong for 115k:

UART_Config(UART0,9600,UART_NO_PARITY,UART_1_StopBits,UARTM_8D);

I guess that´s just a mistake while posting.

The other thing is, which hardware do you use? The STR710-EVAL or own design? On the STR710-EVAL the main oscillator is 16MHz, so you can´t generate a baudrate of 115k without an frequency error of about 15% or something, so the UART of the ARM won´t regognize any start- or stop bits. Try using 14.7456MHz instead as main oscillator. Thereofre have to change the following line in rccu.h then:

#define RCCU_Main_Osc 16000000

to

#define RCCU_Main_Osc 14745600

Regards,

Marcus

hichem2
Associate
June 3, 2005
Posted on June 03, 2005 at 06:27

Hi all,

Thank to all for yours investigation,

ongth60,

You have just to change the following line in your posted code UART_Config(UART0,115200,UART_NO_PARITY,UART_1_StopBits,UARTM_8D);

And ensure that you Configure the UART0 as following:

- Baudrate = 115200Bps

- No parity

- 8 data bits

- 1 stop bit

- No flow control

And your program will work perfectly on the demo board using an external 16MHz oscillator.

I hope that this can help you

With best regards,

Hich :p

ongth60
ongth60Author
Associate III
June 6, 2005
Posted on June 06, 2005 at 07:09

Hi,

Thanks all for trying. Actually the above program can be used for 9600bps as well as 115200bps by changing the baudrate in the following function:

(UART0,115200,UART_NO_PARITY,UART_1_StopBits,UARTM_8D);

or

(UART0,9600,UART_NO_PARITY,UART_1_StopBits,UARTM_8D);

The problem that I'm facing is that I can transmit my ''Hello World'' in the hyperterminal but I cant echo back the characters that I typed in the hyperterminal. From the program, it is suppose to interrupt at UART0 interrupt routine, read the characters typed and transmit the characters to the hyperterminal.

Also, I can detect the ascii character signals typed in the hyperterminal at the RS-232 chip.

So, I would like all to verify if the program can receive the characters type at the hyperterminal to the CPU and CPU transmit them back to the hyperterminal. Then, I will be able to know if the eval board is working or not. Thanks for all the advice.

Rgrds.

hichem2
Associate
June 6, 2005
Posted on June 06, 2005 at 08:25

Hi ongth60,

I try the example and it work perfecly on my eval board (MB393)

I can send you a complete project files if you need it.

Best regards,

Hich :p :-]

ongth60
ongth60Author
Associate III
June 7, 2005
Posted on June 07, 2005 at 10:34

Pls send me the complete project for 115200bps. I will surely need it. Thanks.

Rgrds.

hichem2
Associate
June 7, 2005
Posted on June 07, 2005 at 11:20

Hi ongth60,

Attached you find the asked project,

I hope that this can help you.

with best regards,

Hich ;)

________________

Attachments :

STR71xUART0.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Ie&d=%2Fa%2F0X0000000bm4%2F7Zbpg78KB0soM46rLWoqcS.NPvRxuS2rtx8YnqQekVM&asPdf=false
hichem2
Associate
June 7, 2005
Posted on June 07, 2005 at 11:24

Hi,

the previous project is performed on MB393 demo board.

Cheers,

Hich :o