Skip to main content
hicham
Associate II
Apr 23, 2008 1:59 AM UTC
Question

UART0 (COM1) modem interface

Posted on April 23, 2008 at 03:59

UART0 (COM1) modem interface

This topic has been closed for replies.

1 reply

hicham
hichamAuthor
Associate II
May 17, 2011 7:52 AM UTC
Posted on May 17, 2011 at 09:52

Hi everyone,

The reference manual clearly states on page 253 that UART0 provides a full modem interface. I can clearly see the transmitted data on the oscilloscope on both RX (COM1 Pin 3) and TX (COM1 Pin 2) as well as in their corresponding GPIO pins 3.0 and 3.1. Other than that, I cannot get any signal on any other pin on COM1. Even pin 4 (Data Terminal Ready) which should be high when the UART is enabled is not enabled. As a matter of fact, except RX and TX pins the other pins on the COM1 are not even enabled, as I see on the scope only a ''50Hz noise signal'' similar to the one I get when the scope is powered on but not connected.

I would like to ask you guys if anyone has already tried to actually use the UART0 to communicate with a modem.

My application requires detecting the Ring and DCD signal level changes through interrupts and respond accordingly.

Here is my code, I have made sure that pins were assigned as described by the datasheet

//For Modem interface 2.0 to 2.3 default input functions

GPIO_DeInit(GPIO2);

GPIO_DeInit(GPIO3);

//UART0_Tx pin GPIO3.1 Alternate ouput 2 function

GPIO3->DDR |= 0x02;//output direction

SCU->GPIOOUT[3] |= 0x08; //Alternate ouput 2

//UART0_Rx pin GPIO3.0 Alternate inputs

GPIO3->DDR &= ~0x01;//input direction

SCU->GPIOIN[3] |= 0x01; //Alternate Input

//Pin 3.2 Alternate ouptut 2 UART0_DTR

GPIO3->DDR |= 0x04;//output direction

SCU->GPIOOUT[3] |= 0x30; //Alternate ouput 3

GPIO3->DR[0x3FC] = 0;

UART_InitStructure.UART_WordLength = UART_WordLength_8D;

UART_InitStructure.UART_StopBits = UART_StopBits_1;

UART_InitStructure.UART_Parity = UART_Parity_No ;

UART_InitStructure.UART_BaudRate = 9600;

UART_InitStructure.UART_HardwareFlowControl = ART_HardwareFlowControl_None;

UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx;

UART_InitStructure.UART_FIFO = UART_FIFO_Disable;

//init UART0

UART_DeInit(UART0);

UART_Init(UART0, &UART_InitStructure);

// Enable UART0

UART_Cmd(UART0, ENABLE);

transmission and reception work, my application can communicate with the hyperterminal.

Here is what I observe:

Pin 3.3 (DTR) is high, while COM1 pin 4(DTR) is not enabled

Pins 2.0 (CTS) to 2.3 (Ring indicator) are all high even if a modem is not connected to COM1.

Do you have any explanation?

Any suggestion is much appreciated

Thanx