Skip to main content
jdo
Associate III
October 5, 2023
Question

two stm8s105c6t6 master and slave

Hi! i have two stm8105c6t6 , i want use one to master and other to slave, two pcb board are connect using 10k pull up resistor in the SDA/SCL line.  i am using the example AN3281 stm, but my microcontroller not have tim4, i change the tim4 to tim3 but when i compile the code have the error " not handle interrupt tim3", do you know because this ocurr?

This is the error: "


Running Linker
clnk -m Debug\i2c_master_poll.map -lC:\Lib -o Debug\i2c_master_poll.sm8 Debug\i2c_master_poll.lkf
#error clnk Debug\i2c_master_poll.lkf:1 symbol _TIM2_tout not defined (Debug\i2c_master_poll.o Debug\main.o )
#error clnk Debug\i2c_master_poll.lkf:1 symbol f_TIM4InterruptHandle not defined (Debug\stm8_interrupt_vector.o )
The command: "clnk -m Debug\i2c_master_poll.map -lC:\Lib -o Debug\i2c_master_poll.sm8 Debug\i2c_master_poll.lkf " has failed, the returned value is: 1
exit code=1.

 

TIM4InterruptHandle not defined, but i change tim4 to tim2, and change TIM2InterruptHandle.

 

"

    This topic has been closed for replies.

    1 reply

    AA1
    Senior III
    October 6, 2023

    STM8S105C6T6, the MCU present in STM8S-DISCOVERY board have TIM4 and also TIM1, TIM2, TIM3.

    Maybe you are using the wrong include header file.