Skip to main content
ST Migration account
ST Community Manager
Aug 22, 2026 5:02 PM UTC
Solved

TSC1801 Total output error formula

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.


Dear Team

 

The TSC1801 datasheet contains the following calculation formula.

a5f89f72-127f-b263-9a34-27c8773bddc4.png

What does Voutmeas mean in this formula?

 

Thank you.

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 22, 2026 5:10 PM UTC

Figure 19 is not showing the bidirectional sensing range itself. It shows the output stage drive capability versus output voltage. So the curve does not answer the question 'How does the amplifier measure bidirectionally?', but rather: 'How much current can the output source or sink at which output voltage?'

Is that a bit clearer now?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
ST Technical Moderator
Aug 22, 2026 5:06 PM UTC

Welcome , to the community!

Voutmeas means the measured output voltage at the device OUT pin.
In the formula, it is compared with the ideal output: Vout,ideal = Vsense*Gain + Vref
So Voutmeas is the actual output value you measure on the board, used to calculate the total output error.

Does it answer your question?

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Migration account
ST Community Manager
Aug 22, 2026 5:09 PM UTC

Dear Peter

 

I understand that when sensing in bidirectional mode, the voltage input to Vref is based on a reference of 0A.

Regarding Vref, if Vcc is 5V and Vref is 2.5V, I understand that bidirectional sensing is performed in the range of 0 ~ 2.5V and 2.5V ~ 5V.

However, in Figure 19, it appears that the range fluctuates between 0 and 5V depending on the sink and source.

I do not fully understand this figure; could you please explain it to me?

 

Thank you.

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 22, 2026 5:10 PM UTC

Figure 19 is not showing the bidirectional sensing range itself. It shows the output stage drive capability versus output voltage. So the curve does not answer the question 'How does the amplifier measure bidirectionally?', but rather: 'How much current can the output source or sink at which output voltage?'

Is that a bit clearer now?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.