Skip to main content
irodriguez
Associate II
Jun 15, 2006 11:50 AM UTC
Question

Trying zimage.bin from uClinux package for STR710-EVAL not succesful.

Posted on June 15, 2006 at 13:50

Trying zimage.bin from uClinux package for STR710-EVAL not succesful.

This topic has been closed for replies.

5 replies

irodriguez
Associate II
Jun 1, 2006 6:40 AM UTC
Posted on June 01, 2006 at 08:40

Hi zouh,

I tried what you said. I have uploaded zimage.bin from uClinux package for STR710-EVAL, and I get:

<

Uncompressing Linux...

incomplete literal tree

-- System halted>>

I tried also uploaded this zimage.bin (at 64k offset) and jffs2.img (at 2M offset), with the same result.

irodriguez
Associate II
Jun 8, 2006 7:27 AM UTC
Posted on June 08, 2006 at 09:27

I have tried in another PC with the same result. I'm not able to start downloaded zimage from STR710-EVAL.

Any idea?

irodriguez
Associate II
Jun 8, 2006 11:23 AM UTC
Posted on June 08, 2006 at 13:23

Hi,

I followed application note AN2119, I have dowloaded bootloader into STR710 through REALVIEW JTAG, afterwards I started and configured Hyperterminal, the I saw bootloader information on the Hyperterminal windows after rebooting the Eval Board, I pressed '1' and sent to the board the zimage.bin file, after this I pressed '2' and flashed this image on offset '64k', and finally pressed '3'. All what I get is the error I posted before.

ivo2
Associate
Jun 15, 2006 7:46 AM UTC
Posted on June 15, 2006 at 09:46

Here some hints how to load to image inside evalboard:

1) You should be using latest version of RVDK 1.7

2) Before you start programming the flash memory, you have to connect to

the correct target - ST-STR710-EVAL

3) There is a slight difference between the AN2119 and new RVDK1.7, on

figure three it is written, that you should select 'raw' format for

loading, but in new version you have to select 'rawb' format.

I have attached picture where you can see correct loading of boot loader

inside flash memory.

4) Double check the jumper settings on your board it is mandatory.

5) During step 3.5 Program the Image to External Flash you have to enter following parameters: 64k, 2m

>>>>

Please input the offset of target flash:

64k

Please input the image size(in bytes):

2m

Erasing Block...OK

Programming ... 100%

Verifying...OK

Successfully completed!

<<<<

I have tried it on my side and everything works fine.

Please post us version of SW tools you are using including OS on host computer and terminal application.

On my side I am using RVDK1.7, Hyperterminal on WinXP.

________________

Attachments :

uclinux.gif : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtRh&d=%2Fa%2F0X0000000aQ8%2FAgWvvUPHQ37rmUzjHw8_MHG.is6BgOqt02d7uONLvVg&asPdf=false
irodriguez
Associate II
Jun 15, 2006 11:50 AM UTC
Posted on June 15, 2006 at 13:50

Hi Ivous,

I'm using RVDK 1.7 (I attached an image), with the target you said, ST-STR710-EVAL, I did bootloader upload as you said in your reply, in rawb mode. During Bootloader upload process jumpers SW15 and SW13 are in 2-3 position, and SW14 in 1-2 position. After this, jumpers are set to 2-3 position (SW13,SW14, and SW15).

I entered 64k offset (and 64k offset, 2m size) with the same result.

I'm using Hyperterminal on WinXP (V2002 Service Pack 2).

I have attached screenshots of the entire process and the zimage.bin file, also the bootloader file.

[ This message was edited by: IRU on 15-06-2006 17:23 ]

________________

Attachments :

71xboot-R10.bin : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtRm&d=%2Fa%2F0X0000000aQ9%2F6Vy6yumAtvN9CrlRb1QRcjc_vgHpLSBaHruNjBGpg4g&asPdf=false

Hyperterminal_flash_1.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOe&d=%2Fa%2F0X0000000aPQ%2F6OdInnedvnySzb7AX86XEakNS0IkW9QK_QzRH63XiUI&asPdf=false

Hyperterminal_flash_2.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtRr&d=%2Fa%2F0X0000000aQA%2FTTodrLENAv90mgf8s4u_C_3iJZ0r_ch1lBr2UVV6xQA&asPdf=false

Hyperterminal_sending_zimage_file.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtS1&d=%2Fa%2F0X0000000aQB%2FeA4RVaQAeJrveMj2JIrFHtLOlBBenLeRgEXbz9ZBIcA&asPdf=false

RealView.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOL&d=%2Fa%2F0X0000000aPM%2FHFKl_MBAr8qixvQRnJPutjqoEJBVxQx_wnEMZWYSCB4&asPdf=false

RealView_Uploaded.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtN3&d=%2Fa%2F0X0000000aP7%2FDXTXPmPXDP4W5dxCD2PdAcduit6yHc3Gicl0hsPACgU&asPdf=false

RealView_Uploading.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtS6&d=%2Fa%2F0X0000000aQC%2Ff.XitgjX1osh9Iyr6unZC.IKQI2k0rKbDBCJpPi08rQ&asPdf=false

zimage.bin : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtPn&d=%2Fa%2F0X0000000aPg%2FaOWOVc3oBbgLZ_eUxo5nOto41pPGd3jXF8QT0hPLitk&asPdf=false