Skip to main content
Chayan Roy
Associate III
Mar 1, 2017 11:09 AM UTC
Question

Timer4 not respohding as expected

Posted on March 01, 2017 at 12:09

Hello,

  I am trying to  make a 200us pulse,using simple time dealy.  I am using TIMER4 to create delay. But the problem is whatever prescalar I  use or  What ever Autoreload value I have timer always gives 12us pulse.  I am using stm8s003f3p6 controller.

Code is below:

#include 'STM8S003F3P.h'

void InitialiseSystemClock(void);

void InitialiseSystemClock(void)

{

CLK_ICKR = 0; // Reset the Internal Clock Register.

CLK_ICKR = (1<<0);; // Enable the HSI.

CLK_ECKR = 0; // Disable the external clock.

while (!(CLK_ICKR & (1<<1))); // Wait for the HSI to be ready for use.

CLK_CKDIVR = 0; // Ensure the clocks are running at full speed.

CLK_PCKENR1 = 0xff; // Enable all peripheral clocks.

CLK_PCKENR2 = 0xff; // Ditto.

CLK_CCOR = 0; // Turn off CCO.

CLK_HSITRIMR = 0; // Turn off any HSIU trimming.

CLK_SWIMCCR = 0; // Set SWIM to run at clock / 2.

CLK_SWR = 0xe1; // Use HSI as the clock source.

CLK_SWCR = 0; // Reset the clock switch control register.

CLK_SWCR = (1<<1); // Enable switching.

while (CLK_SWCR & (1<<0)); // Pause while the clock switch is busy.

}

void main(void){

InitialiseSystemClock();

PD_DDR |=(1<<1);

PD_CR1 |=(1<<1);

PD_CR2 |=(1<<1);

TIM4_PSCR=16;

TIM4_ARR=255;

TIM4_IER=(1<<0);

TIM4_CR1=(1<<0);

_asm('rim');

while(1){

}

}

@far @interrupt void TIMER4_INTERRUPT (void){

PD_ODR^=(1<<1);

TIM4_SR &=~(1<<0);

return;

}

    This topic has been closed for replies.