Skip to main content
vcelik
Associate II
Jun 15, 2010 9:07 AM UTC
Question

Timer1 Triggered and Scan Mode ADC1

Posted on June 15, 2010 at 11:07

Timer1 Triggered and Scan Mode ADC1

    This topic has been closed for replies.

    7 replies

    vcelik
    vcelikAuthor
    Associate II
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    Yes. 

    ADC1_ConversionConfig() function must come after the ADC1_Cmd(ENABLE),

    ADC1_ScanModeCmd(ENABLE) and 

    ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE) functions.

    Because these functions reset the channel definition of the

    ADC1->CSR register.

    So the right initiation function is like this:

    void MyInitFunc(void)

    {

          

    ADC1_Cmd(ENABLE);    

    ADC1_ScanModeCmd(ENABLE);  

    ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);

    ADC1_ConversionConfig(ADC1_CONVERSIONMODE_SINGLE, ADC1_CHANNEL_8, ADC1_ALIGN_RIGHT);

    ADC1_PrescalerConfig(ADC1_PRESSEL_FCPU_D2);

        

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL0, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL1, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL2, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL3, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL4, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL5, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL6, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL7, DISABLE);

    ADC1_SchmittTriggerConfig(ADC1_SCHMITTTRIG_CHANNEL8, DISABLE);

      

        TIM1_SelectMasterSlaveMode(ENABLE);   

        ADC1_ExternalTriggerConfig(ADC1_EXTTRIG_TIM, ENABLE); 

        

    TIM1_TimeBaseInit(3999, TIM1_COUNTERMODE_UP, 4000, 0);        

        

    TIM1_SelectOutputTrigger(TIM1_TRGOSOURCE_UPDATE); 

        

    TIM1_Cmd(ENABLE);

    }

    sylvain_laurent
    Associate II
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    Hi volkan,

    Yesterday, I tested your code with my demo board because I would like to use the same purpose in my project.

    First of all, without use interrupt and timer1 trigger so i'm in pulling mode, the conversions are good on all ADC inputs.

    But after, with interrupt on EOC, I have the same problem.

    Only the first [0] get values.

    Do you resolved your problem ?

    Thanks.

    mchnani
    Associate
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    Hi Volkan,

    I use STMS105K4 (COSMIC) and i would like to use seven channels with scan mode. When i tested your final code i have errors with ADC1

    The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib''

    What's the library are you used in your project, 

    Thank you in advance

    Best regards,

    sylvain_laurent
    Associate II
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    Hi,

    Good job, this code run very well.

    Thanks.

    sylvain_laurent
    Associate II
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    Ok thanks for all,

    I think tomorrow, I'll try your code in my project.

    Thanks yet, regards.

    lowpowermcu
    Associate III
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    Hi moussa,

    ''CXSTM8_16K'' means that he is using cosmic compiler with limited code size to 16K.

    regards,

    MCU Lüfter

    eos1d3
    Associate II
    May 17, 2011 1:09 PM UTC
    Posted on May 17, 2011 at 15:09

    I believe you need the following before enabling ADC1:

    ADC1_DataBufferCMD(ENABLE);

    https://my.st.com/public/STe2ecommunities/mcu/Lists/STM8/group__ADC1__Public__Functions.html#ge1604ac905b2237098c53046e100f679