Skip to main content
ohadr2
Associate II
May 25, 2006 8:59 PM UTC
Question

timer interrupt routine problem COSMIC compiler

Posted on May 25, 2006 at 22:59

timer interrupt routine problem COSMIC compiler

This topic has been closed for replies.

4 replies

ohadr2
ohadr2Author
Associate II
May 4, 2006 3:03 AM UTC
Posted on May 04, 2006 at 05:03

hello

i wrote a program that operate the timer as a counter.

in intetion to create an interrupt.

there are 3 problems:

1) the TCHR and TCLR are not going up only the TACR

2) the TOF register never occure never set to 1.

3) I alwys enter the interrupt routine

and I can not go out from it.

My program is:

#include

#define output 1

#define input 0

#define EnableInterrupts _asm(''RIM'')

#define DisableInterrupts _asm(''SIM'')

void main()

{

EnableInterrupts;

TCR1=0b00100000; //configure the counter

TCR2=0b00000100;

TCSR=0b00000100;

TCLR=0; //restat the counter to 650000

//TCSR=0b00000000;

while(1)

{

}

}

and th INPERRUPT:

extern void _stext(); /* startup routine */

//extern unsigned char ohad;

@interrupt void INT_Timer(void)

{

//return;

char t2=9;

t2=10;

t2=11;

}

/* Interrupt vector table, to be linked at the address

0xFFE0 (in ROM) */

void (* const _vectab[])() = {

INT_Timer, /* 0xFFE0 */

INT_Timer, /* 0xFFE2 */

INT_Timer, /* 0xFFE4 */

INT_Timer, /* 0xFFE6 */

INT_Timer, /* 0xFFE8 */

INT_Timer, /* 0xFFEA */

INT_Timer, /* 0xFFEC */

INT_Timer, /* 0xFFEE */

INT_Timer, /* 0xFFF0 */

INT_Timer, /* 0xFFF2 */

INT_Timer, /* 0xFFF4 */

INT_Timer, /* 0xFFF6 */

INT_Timer, /* 0xFFF8 */

INT_Timer, /* 0xFFFA */

INT_Timer, /* Trap vector */

_stext, /* Reset Vector */

};

luca239955_st
Associate II
May 4, 2006 4:26 AM UTC
Posted on May 04, 2006 at 06:26

Hello,

from the compiler point of view, I see no problems with your code.

When you say ''I never get out of the interrupt routine'', it's more likely that you actually get out (execute RETI), but then immediately get back into it again because another interrupt happens (you did'n clear the flag, or another interrupt source is active...)

Regards,

Luca (Cosmic)

ohadr2
ohadr2Author
Associate II
May 4, 2006 5:11 AM UTC
Posted on May 04, 2006 at 07:11

Hello Luca

Can u tell me how do i clear the Interrupt Flag??

after I get in to interrupt routine i have added:

@interrupt void TIMER_int (void)

{

char ohad1=0;

ohad1=1l;

ohad1=12;

ohad1=TCSR;

TCLR=0;

}

when I look into the VIEW-->Peripheral Register I can not see

the TOF flag at all.

so can you tell how do i get out from thsu interrupt??

I suspect that the TOF is still set or i did not put IRET instruction

thanks

ohad

mjg21cn
Visitor II
May 25, 2006 8:59 PM UTC
Posted on May 25, 2006 at 22:59

I think you should not put all interrupt to INT_Timer,maybe you can write one interrupt routine for every interrupt. then you will find where work wrong.

do you think so.

regards.