Skip to main content
klaasdc
Associate III
Jun 13, 2012 7:02 PM UTC
Question

Timer as frequency/RPM counter, CapCom offset?

Posted on June 13, 2012 at 21:02

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    2 replies

    klaasdc
    klaasdcAuthor
    Associate III
    Jun 27, 2012 7:31 PM UTC
    Posted on June 27, 2012 at 21:31

    Has no one used a timer to measure input signals?

    :(

    klaasdc
    klaasdcAuthor
    Associate III
    Jun 27, 2012 8:26 PM UTC
    Posted on June 27, 2012 at 22:26

    Could it be that the timer misses a few ''counts'' after it is being reset in Slave Mode? (TIM1_SLAVEMODE_RESET)

    That would explain why I always end up with frequency values that are too high (or periods that are too low for that matter)....