Skip to main content
egesuita
Associate II
Aug 9, 2005 4:39 AM UTC
Question

TIMER A on ST72F324J6B5

Posted on August 09, 2005 at 06:39

TIMER A on ST72F324J6B5

This topic has been closed for replies.

2 replies

egesuita
egesuitaAuthor
Associate II
Jul 11, 2005 10:39 AM UTC
Posted on July 11, 2005 at 12:39

hi everybody,

I'm developing firmware for a ST72F324J6 (42pin sdip package) microcontroller.

I want to generate a pwm waveform with timer A and applied it to pin OCMP1_A (pin 13).

attached you'll find the C code I wrote down.

just for test purposes the duty cycle is approx 50%.

the code do not produce the expected result: no pwm appear on OCMP1_A pin.

I checked several times the few line of code i posted here but i'm not able to find the bug in them.... pehaps some missing sttings... I followed step by step what I found on the ST72F324 manual.... I think my error is naive but I can't find it!

macro I used for setting and resetting bits (_bset & _bres) are tested and functioning.

any suggestion ??

thanks a lot for your precious help

regards

________________

Attachments :

timerA.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzuq&d=%2Fa%2F0X0000000bTi%2FeCXQDSOKlvA93faDFwjM9TVmh8tvRPzTIzGi8.F7.wE&asPdf=false
jatin
Visitor II
Aug 9, 2005 4:39 AM UTC
Posted on August 09, 2005 at 06:39

It is difficult to suggest something from your attached code. The best way is to use the ST7 software libarary containing the 16-bit timer peripheral. It can be downloaded from the same site.