Skip to main content
Nevyn
Associate III
Sep 4, 2012 12:41 PM UTC
Question

Timer 1, Channel 3 Lower Than Expected Output Voltage

Posted on September 04, 2012 at 14:41

I have been developing some applications for the STM8S103F3 which I have on breadboard and I have recently transferred one of the projects to the STM8S Discovery board and I am finding a difference in behaviour which I cannot work out.

The program uses PWM Mode 2 to output a 60 uS square wave on timer 1 channel3.  On the STM8S103F3 on breadboard the program works fine and I get a 0 to 3.3V square wave.

On the Discovery board I have the square wave with the right frequency but the output voltage is only 280 mV peak-to-peak.  The only things I have connected to the Discovery board are the USB connection and the scope connected to the timer output and ground.

I am using IAR as the development environment and I have modified the include files and project options accordingly.

Any ideas where I could be going wrong? Am I correct in assuming that if the app runs on the STM8S103F3 then it will run on the Discovery board assuming I change the include file and target chip?

The code for the application is included below.

Regards,

Mark

&sharpinclude <intrinsics.h>

&sharpinclude <iostm8s103f3.h>

//

//  Setup the system clock to run at 16MHz using the internal oscillator.

//

void InitialiseSystemClock()

{

    CLK_ICKR = 0;                       //  Reset the Internal Clock Register.

    CLK_ICKR_HSIEN = 1;                 //  Enable the HSI.

    CLK_ECKR = 0;                       //  Disable the external clock.

    while (CLK_ICKR_HSIRDY == 0);       //  Wait for the HSI to be ready for use.

    CLK_CKDIVR = 0;                     //  Ensure the clocks are running at full speed.

    CLK_PCKENR1 = 0xff;                 //  Enable all peripheral clocks.

    CLK_PCKENR2 = 0xff;                 //  Ditto.

    CLK_CCOR = 0;                       //  Turn off CCO.

    CLK_HSITRIMR = 0;                   //  Turn off any HSIU trimming.

    CLK_SWIMCCR = 0;                    //  Set SWIM to run at clock / 2.

    CLK_SWR = 0xe1;                     //  Use HSI as the clock source.

    CLK_SWCR = 0;                       //  Reset the clock switch control register.

    CLK_SWCR_SWEN = 1;                  //  Enable switching.

    while (CLK_SWCR_SWBSY != 0);        //  Pause while the clock switch is busy.

}

//

//  Initialise Timer 1.

//

void InitialiseTimer1()

{

    TIM1_CR1 = 0;

    TIM1_CR2 = 0;

    TIM1_SMCR = 0;

    TIM1_ETR = 0;

    TIM1_IER  = 0;

    TIM1_SR2  = 0;

    TIM1_CCER1 = 0;

    TIM1_CCER2 = 0;

    TIM1_CCMR1 = 0;

    TIM1_CCMR2 = 0;

    TIM1_CCMR3 = 0;

    TIM1_CCMR4 = 0;

    TIM1_CCER1 = 0;

    TIM1_CCER2 = 0;

    TIM1_CCMR1 = 0;

    TIM1_CCMR2 = 0;

    TIM1_CCMR3 = 0;

    TIM1_CCMR4 = 0;

    TIM1_CNTRH = 0;

    TIM1_CNTRL = 0;

    TIM1_PSCRH = 0;

    TIM1_PSCRL = 0;

    TIM1_ARRH  = 0;

    TIM1_ARRL  = 0;

    TIM1_CCR1H = 0;

    TIM1_CCR1L = 0;

    TIM1_CCR2H = 0;

    TIM1_CCR2L = 0;

    TIM1_CCR3H = 0;

    TIM1_CCR3L = 0;

    TIM1_CCR4H = 0;

    TIM1_CCR4L = 0;

    TIM1_OISR  = 0;

    TIM1_EGR   = 0x01;

    TIM1_DTR   = 0;

    TIM1_BKR   = 0;

    TIM1_RCR   = 0;

    TIM1_SR1   = 0;

}

//

//  Set up Timer 1, channel 3 to output a single pulse lasting 30 uS.

//

void SetupTimer1()

{

    TIM1_ARRH = 0x03;       //  Reload counter = 960

    TIM1_ARRL = 0xc0;

    TIM1_PSCRH = 0;         //  Prescalar = 0 (i.e. 1)

    TIM1_PSCRL = 0;

    TIM1_CR1_DIR = 0;       //  Up counter.

    TIM1_CR1_CMS = 0;       //  Edge aligned counter.

    TIM1_RCR = 0;           //  No repetition.

    //

    //  Now configure Timer 1, channel 3.

    //

    TIM1_CCMR3_OC3M = 7;    //  Set up to use PWM mode 2.

    TIM1_CCER2_CC3E = 1;    //  Output is enabled.

    TIM1_CCER2_CC3P = 0;    //  Active is defined as high.

    TIM1_CCR3H = 0x01;      //  480 = 50% duty cycle (based on TIM1_ARR).

    TIM1_CCR3L = 0xe0;

    TIM1_BKR_MOE = 1;       //  Enable the main output.

//    TIM1_CR1_OPM = 1;

    TIM1_CR1_CEN = 1;

}

//

//  Main program loop.

//

void main()

{

    //

    //  Initialise the system.

    //

    __disable_interrupt();

    InitialiseSystemClock();

    InitialiseTimer1();

    SetupTimer1();

    __enable_interrupt();

    while (1)

    {

        __wait_for_interrupt();

    }

}

#stm8s103f3-discovery-timer
    This topic has been closed for replies.

    2 replies

    Nevyn
    NevynAuthor
    Associate III
    Oct 6, 2012 9:37 AM UTC
    Posted on October 06, 2012 at 11:37

    Worked this one out (with the help from a friend).  The problem is that the pin outputting the Tim1Ch3 signal is connected to the touch sensor.  I changed the channel to Tim1Ch4 and everything is looking good.

    I could have removed the connection as the manual tells you how to do this but I thought I'd try the non-invasive route first.

    Regards,

    Mark
    Aaron Derbyshire
    Associate III
    Jul 4, 2017 11:38 AM UTC
    Posted on July 04, 2017 at 13:38

    hi,

    I am having a similar issue with Timer 2, channel 2 on Port D Pin 3.

    I've double checked the schematic fir the STM8S discovery board and this pin is unused.

    My timer configuration is as follows:

    void TIM2_PWM(void)

    {

     /* SET PRESCALER */

     TIM2.PSCR = 0;

     /* SET ARR */

     TIM2.ARRH = 0x4E;

     TIM2.ARRL = 0x1F;

     /* CH1 ENABLED ACTIVE LOW POLARITY */

     TIM2.CCER1 = 0x30;

     /* PWM2 */

     TIM2.CCMR2 = 0x70;

     /* SET PULSE WIDTH */

     TIM2.CCR2H = 0x3E;

     TIM2.CCR2L = 0x80;

     /* ENABLE PRELOAD REGISTER */

     TIM2.CCMR2 |= 0x08;

     /* TIM2_ARR PRELOAD ENABLE */

     TIM2.CR1 |= 0x80;

     /* TIM2 ENABLE */ 

     TIM2.CR1 |= 0x01;

    }

    The resulting output is generating a 800Hz signal with a 80% duty cycle, as desired. However, the waveform is peaking at 360mV. I have that pin configured as a push-pull output at 10Mhz.

    Any help would be greatly appreciated.

    Regards

    Aaron