Skip to main content
nataliap
Visitor II
Oct 26, 2014 2:40 PM UTC
Question

TIM1 TRGO FOR ADC

Posted on October 26, 2014 at 15:40

I work on ST-Microcontroller  :STM8S003F3U6.

I try to use TIM1 as a trigger (TRGO) for ADC interrupt.

When I use the single pulse (TIM1_CR1_OPM=1)   mode (on TIM1 counter overflow) everything seems to work well,

but when I change TIM1_CR1_OPM to ''0'' for counter's continuous work, the ADC interrupt stops working.

TIM1 no longer launch ADC at the TIM1-counter overflow.

I need TIM1-counter work continuously and start ADC at every TIM1-counter overflow.

I don’t understand what am I doing wrong?

the relevant parts of my code:

//*******ADC + TIM1**  init  ******************************/

//********************************************************/

 

  ADC_CSR_EOC=0;

 

ADC_CR1_ADON=0;         // power OFF ADC

  ADC_CR1_SPSEL=ADCPS;    // sampling rate

  ADC_CR2_ALIGN=1;        // right align

  ADC_CSR_CH=4;           // point to  channel

 

  ADC_CR2_EXTSEL=0;     //Internal TIM1 TRGO event

  ADC_CR2_EXTTRIG=1;    //Conversion on external event disabled

 

  ADC_CSR_EOCIE=1;         //end of conversion interrupt enable

 

  TIM1_PSCRH=0x00;         // set prescaler

  TIM1_PSCRL=0x10;         // 1MHz

  TIM1_ARRH=0x00;          //00 // set irq reriod

  TIM1_ARRL=0x08; 

   

  TIM1_CR1_URS=TRUE;      //gen timer irq on overflow only 

  TIM1_IER_TIE=1;         //enable TRIG  irq

  TIM1_CR2_MMS=0x01;     //enable master mode

 

 

TIM1_CR1_OPM=0;              //

Counter is not stopped at update event

 

  

ADC_CR1_ADON=1;

  

  

  __enable_interrupt();

/********************************************************/

/*                      MAIN                                                                            */

/********************************************************/

void main(void)

{

        

       

TIM1_CR1_CEN=TRUE;        //enable Timer1 counter

   

 

   /* Loops 'forever', taking input when interrupted. */

while (1)

   {  }

}

/***********************************************************************/

/* Defines an interrupt handler for the ADC vector                                                            */

/***********************************************************************/

#pragma vector=ADC_VECTOR

__interrupt __root void ADCHandler(void)

{

     

 while (ADC_CSR_EOC==0) {}

                  

                     ADC_CSR_EOC=0;   //End of conversion

   

 

TIM1_SR1_UIF=0;            // rset pending irq

}

Help!!

    This topic has been closed for replies.