Skip to main content
November 1, 2022
Question

TIM1 jumping count in the encoder mode

I'm using a TTC encoder connected to stm8s003f . TIM1 counts correctly until it reaches the value before the overflow value . After that it either jumps to 0 or it shows the overflow value. What is that due to?Thank you.

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 1, 2022

    What's the maximal value of the TIM configured too? Show code.

    ​

    Is the overflow just an alert, or does it have secondary consequences?​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    November 2, 2022

    void Filter_Value(uint8_t value);

    void clock_setup(void);

    void GPIO_setup(void);

    unsigned int present_value = 0x0000;

    unsigned int previous_value = 0x0000;

    void TIM1_setup(void);

    void main(void)

    {

      clock_setup();

      GPIO_setup();

      TIM1_setup();

      /* Infinite loop */

       while(1){

        present_value = TIM1_GetCounter()/2;

        if(present_value != previous_value)

           GPIO_WriteReverse(GPIOA, GPIO_PIN_1);

        previous_value = present_value;

      }   

    }

    void TIM1_setup(void){

      TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_UP, 10, 0);

      TIM1_EncoderInterfaceConfig(TIM1_ENCODERMODE_TI12, TIM1_ICPOLARITY_RISING, TIM1_ICPOLARITY_RISING);

      enableInterrupts();

      Filter_Value(0);

      TIM1_Cmd(ENABLE);

    }

    void Filter_Value(uint8_t value){

     TIM1->CCMR1|=(uint8_t)(value<<4);

     TIM1->CCMR2|=(uint8_t)(value<<4); 

    }

    void clock_setup(void)

    {

        CLK_DeInit();

        CLK_HSECmd(DISABLE);

        CLK_LSICmd(DISABLE);

        CLK_HSICmd(ENABLE);

        while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == 0);

        CLK_ClockSwitchCmd(ENABLE);

        CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);                     

        CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);

        CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, DISABLE,

        CLK_CURRENTCLOCKSTATE_ENABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_I2C, DISABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, ENABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_SPI, DISABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, DISABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_AWU, DISABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART1, DISABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, DISABLE);

        CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER4, DISABLE);

    }

    void GPIO_setup(void)

    {

        GPIO_DeInit(GPIOC);

        GPIO_Init(GPIOC,

             ((GPIO_Pin_TypeDef)(GPIO_PIN_7 | GPIO_PIN_6)),

             GPIO_MODE_IN_PU_NO_IT); 

        GPIO_DeInit(GPIOA);

        GPIO_Init(GPIOA, GPIO_PIN_1, GPIO_MODE_OUT_PP_HIGH_SLOW);

        

    }

    AA1
    Senior III
    November 3, 2022

    If you read RM0016 page 185, it seems what you said, is the correct behavior.

    The counter counts continuously between 0 and the auto-reload value in the TIM1_ARR register (0 to ARR or ARR down to 0 depending on the direction).