Skip to main content
Jhabi
Associate
January 12, 2020
Question

TIM1 doesn't work on STM8S003F3PU

Hello

I'm Using STM8S003F3PU mini-eval Board. My software is STVD and Cosmic.

Why My TIM1 don't work truly? It should measure the input signal HIGH_Duration on TIM1_CH1 (= PC6) and my led on PA3 turned off. But that's not so. Furthermore, I use debug mode but it doesn't enter my condition( if(duty_cycle_updated))

Main.c:

 #include "stm8s.h"
 
 
 //Pulse width measurment
 unsigned char data_value;
 unsigned long duty_cycle = 0;
 unsigned long duty_cycle_temp = 0;
 
 unsigned long start_time = 0;
 unsigned long end_time = 0;
 bool duty_cycle_updated=FALSE;
 bool state=FALSE;
 void clock_setup(void);
 void GPIO_setup(void);
 void TIM1_setup(void);
 void TIM2_setup(void);
 void delay_cycles(uint16_t cy);
 
 void main() {
 //Set PinMode
 
 GPIOA->DDR |= 0xFF; // PD.0 as Output
 GPIOA->CR1 |= 0xFF; // PD.0 as Push Pull Type Output
 		 GPIOA->ODR |=1ODR &= ~(1

stm8s_it.c:(Top part only)

 

 #include "stm8s_it.h"
 #include "stm8s_eval.h"
 #include "stm8s.h"
 
 static bool state = FALSE;
 extern unsigned long duty_cycle;
 extern unsigned long start_time;
 extern unsigned long end_time;
 static bool duty_cycle_updated=FALSE;
 
 unsigned long my_test_****=0;
 
 void TIM1_CH1_OVF_IRQHandler(void){
 my_test_****++;
 }
 
 
 void TIM1_CH1_CCP_IRQHandler(void){
 if(TIM1_GetFlagStatus(TIM1_FLAG_CC1)) {
 if(state == FALSE) {
 start_time = TIM1_GetCapture1();
 TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_FALLING, TIM1_ICSELECTION_DIRECTTI, 1, 1);
 }
 else {
 end_time = TIM1_GetCapture1();
 TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI, 1, 1);
 duty_cycle = (end_time - start_time);
 							duty_cycle_updated=TRUE;
 }
 state = ~state;
 }
 TIM1_ClearITPendingBit(TIM1_IT_CC1);
 TIM1_ClearFlag(TIM1_FLAG_CC1);
 }

stm8s_interupt_vector:

 

 #include "stm8s_it.h"
 
 typedef void @far (*interrupt_handler_t)(void);
 
 struct interrupt_vector {
 	unsigned char interrupt_instruction;
 	interrupt_handler_t interrupt_handler;
 };
 
 @far @interrupt void NonHandledInterrupt (void)
 {
 	/* in order to detect unexpected events during development, 
 	 it is recommended to set a breakpoint on the following instruction
 	*/
 	return;
 }
 
 extern void _stext(); /* startup routine */
 
 struct interrupt_vector const _vectab[] = {
 	{0x82, (interrupt_handler_t)_stext}, /* reset */
 	{0x82, NonHandledInterrupt}, /* trap */
 	{0x82, NonHandledInterrupt}, /* irq0 */
 	{0x82, NonHandledInterrupt}, /* irq1 */
 	{0x82, NonHandledInterrupt}, /* irq2 */
 	{0x82, NonHandledInterrupt}, /* irq3 */
 	{0x82, NonHandledInterrupt}, /* irq4 */
 	{0x82, NonHandledInterrupt}, /* irq5 */
 	{0x82, NonHandledInterrupt}, /* irq6 */
 	{0x82, NonHandledInterrupt}, /* irq7 */
 	{0x82, NonHandledInterrupt}, /* irq8 */
 	{0x82, NonHandledInterrupt}, /* irq9 */
 	{0x82, NonHandledInterrupt}, /* irq10 */
 	{0x82, (interrupt_handler_t)TIM1_CH1_OVF_IRQHandler}, /* irq11 */
 {0x82, (interrupt_handler_t)TIM1_CH1_CCP_IRQHandler}, /* irq12 */
 	{0x82, NonHandledInterrupt}, /* irq13 */
 	{0x82, NonHandledInterrupt}, /* irq14 */
 	{0x82, NonHandledInterrupt}, /* irq15 */
 	{0x82, NonHandledInterrupt}, /* irq16 */
 	{0x82, NonHandledInterrupt}, /* irq17 */
 	{0x82, NonHandledInterrupt}, /* irq18 */
 	{0x82, NonHandledInterrupt}, /* irq19 */
 	{0x82, NonHandledInterrupt}, /* irq20 */
 	{0x82, NonHandledInterrupt}, /* irq21 */
 	{0x82, NonHandledInterrupt}, /* irq22 */
 	{0x82, NonHandledInterrupt}, /* irq23 */
 	{0x82, NonHandledInterrupt}, /* irq24 */
 	{0x82, NonHandledInterrupt}, /* irq25 */
 	{0x82, NonHandledInterrupt}, /* irq26 */
 	{0x82, NonHandledInterrupt}, /* irq27 */
 	{0x82, NonHandledInterrupt}, /* irq28 */
 	{0x82, NonHandledInterrupt}, /* irq29 */
 };

stm8s_it.h(top part only):

 

 #ifndef __STM8S_IT_H
 #define __STM8S_IT_H
 @far @interrupt void TIM1_CH1_OVF_IRQHandler(void);
 @far @interrupt void TIM1_CH1_CCP_IRQHandler(void);
 
 
 /* Includes ------------------------------------------------------------------*/
 #include "stm8s.h"
 
 

 

    This topic has been closed for replies.