Skip to main content
mateuszficek
Associate
Mar 8, 2012 7:57 PM UTC
Question

TIM1 counter

Posted on March 08, 2012 at 20:57

Hello,

I try

measure

frequency

50-500Hz. I use STM8S-DISCOVERY KIT with STM8S105C6T6 and FWLib. How

initiate

the appropriate

timer and

which port

to use

?

#include ''stm8s_conf.h''
#include ''stm8s.h''
#include ''stm8s_it.h''
#include ''stm8s_tim1.h''
#include ''stm8s_gpio.h''
void
init(
void
);
void
GPIO_app_init(
void
);
void
TIM1_app_init(
void
);
main()
{
init();
enableInterrupts();
while
(1)
{
TIM1_SetCounter(5); 
tim1freq = TIM1_GetCounter();
}
}
void
init(
void
)
{
GPIO_app_init();
TIM1_app_init();
return
;
}
void
GPIO_app_init(
void
)
{
}
void
TIM1_app_init()
{
TIM1_DeInit();
TIM1_TimeBaseInit(31, TIM1_COUNTERMODE_UP, 65535, 0)
TIM1_CounterModeConfig (TIM1_COUNTERMODE_UP);
//TIM1_ICInit(TIM1_CHANNEL_1,TIM1_ICPOLARITY_RISING,TIM1_ICSELECTION_DIRECTTI,TIM1_

    This topic has been closed for replies.

    2 replies

    Nickname13136_O
    Visitor II
    Mar 13, 2012 12:24 PM UTC
    Posted on March 13, 2012 at 13:24

    Pls refer STM8S105C6T6 datasheet and STM8S-DISCOVERY KIT  UM for proper selection of GPIO.

    Regards,

    mateuszficek
    Associate
    Mar 13, 2012 6:29 PM UTC
    Posted on March 13, 2012 at 19:29

    In this way?

    what

    to do next

    ,

    to measure

    frequency (50Hz- 500kHz)

    .

    void GPIO_app_init(void)
    {
    GPIO_DeInit(GPIOC);
    GPIO_Init(GPIOC, GPIO_PIN_
    1
    , GPIO_MODE_IN_FL_NO_IT);
    }