Skip to main content
Associate II
October 13, 2025
Question

The issue about the PD55008-E

Hi,i meeting a issue,

bobber_0-1760327433434.png

I suspect that the parasitic capacitance from the PD55008-E is too large?

bobber_1-1760327815243.png

The waveform output from J500 and the edge is shaking too much.

Thanks!

This topic has been closed for replies.

3 replies

bobberAuthor
Associate II
October 13, 2025

Are there any other options? For example, replacement plan...

Peter BENSCH
ST Technical Moderator
October 13, 2025

So far, apart from the schematic extract, you have only mentioned a few marginal parameters and no layout details.

The ringing observed at 15MHz when switching off (?) can be caused, for example, by line inductance in addition to L501 together with the parallel capacitors C507 and C506.

What do you mean by ‘replacement plan’?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
bobberAuthor
Associate II
October 14, 2025

Hi Peter,

The first,thank you for your support.

I understand what you mean now.

This is Layout picture:

bobber_0-1760419406147.png

The signal frequency is 40 MHz output from J500,but I'm pretty sure I won't be able to modify the layout.

The 'replacement plan' is replace PD55008-E with a smaller parasitic capacitance MOSFET.

Thanks

Best reagrds

Xingqi