Skip to main content
Associate
Jun 15, 2024 5:17 AM UTC
Solved

"The interface firmware FAILED to reset/halt the target MCU" .txt with STEVAL-SPIN3202

Hello,

I am working with STEVAL-SPIN3202 to develop motor control solution. I am using the Motor Control Workbench 6.2.1. 

I could generate the project using the workbench, however when i Connect the evaluation board, window with FAIL.txt opens which reads "The interface firmware FAILED to reset/halt the target MCU".

Thus I am not able to connect to the board. I have tried connecting to the board using ST-Link Utility, however it gives the error message "Can not connect to target".

I have tried some of the solution mentioned on the forum but the issue still persist.

Please guide me so that i can get my motor running.

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
Jun 15, 2024 8:51 AM UTC

To the board...see manual:

AScha3_0-1718441499041.png

 

If you feel a post has answered your question, please click on " Best Answer ".

8 replies

AScha.3
Super User
Jun 15, 2024 6:48 AM UTC

Hi,

ST-Link Utility is old, deprecated. Dont use this .

So try with CubeProgrammer , connect "under reset" or "software reset" .

 

If you feel a post has answered your question, please click on " Best Answer ".
D_AnkitAuthor
Associate
Jun 15, 2024 7:03 AM UTC

Hi,

Thank you for your reply. Tried with CubeProgrammer. Still no luck. It throws below error and when the board is connected FAIL.txt is still generated.ST_error.png

AScha.3
Super User
Jun 15, 2024 7:29 AM UTC

Hi,

"no target found" is just info: cannot connect...

So show, what CubeProgrammer shows...target voltage...etc.

so:

AScha3_0-1718436545102.png

 

If you feel a post has answered your question, please click on " Best Answer ".