Skip to main content
Visitor II
July 4, 2023
Question

The controller jumps into ISR only one time and comes out immediately and executes other functionali

I am using STM8AF62A9. 

I reconfigured the interrupt vector table, unused interrupts and tests it with TRAP SW with function __trap();

Controller jumps into the unhandled interrupt ISR routine, as expected, but in there i doesn't clear the interrupt flag.
Expectation was that controller would remain stuck in ISR loop or continuously jump into the ISR routine and will not execute other part of code, but actually the controller jumps into ISR only one time and comes out immediately and executes other functionality.

Is flag should be reset? Can you please share the full datasheet pointing interrupt vector table? 

Or did i missed something?

  

    This topic has been closed for replies.

    1 reply

    AA1
    Senior III
    July 5, 2023

    TRAP doesn't have interrupt clear flag.TRAP ISR is executed once for each TRAP instruction. After return from ISR program continues after the TRAP instruction.