Skip to main content
DanielGouvea
Associate
Mar 17, 2026 10:35 PM UTC
Solved

TDA7293V Mute/ST-BY Control Range for High Voltage Design

Dear Support Team,
I am planning to implement a circuit based on the TDA7293V. In this design, the IC will remain powered on, so I intend to use the circuit shown in Figure 6 (Single signal standby/mute control circuit) to prevent 'pop' noise. Given that my supply rails are ±44V (+Vs = +44V and -Vs = -44V), what is the recommended voltage range for the MUTE/ST-BY signal to ensure reliable operation?
Thanks in advance!! With warm regards, Daniel.

 

MUTE_STDBY.png

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Mar 19, 2026 9:51 AM UTC

STBY and MUTE voltages of up to (+Vs)+|(-Vs)| can be applied, in your case 88V (referenced to Vs-) or 44V (referenced to GND).

However, since both inputs switch between a maximum of 1.5V (switch-on threshold) and a minimum of 3.5V (switch-off threshold), a control voltage referenced to Pin 1, typically GND, close to 0V is appropriate for the activated state and 4...5V for the deactivated state.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Mar 19, 2026 9:51 AM UTC

STBY and MUTE voltages of up to (+Vs)+|(-Vs)| can be applied, in your case 88V (referenced to Vs-) or 44V (referenced to GND).

However, since both inputs switch between a maximum of 1.5V (switch-on threshold) and a minimum of 3.5V (switch-off threshold), a control voltage referenced to Pin 1, typically GND, close to 0V is appropriate for the activated state and 4...5V for the deactivated state.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DanielGouvea
Associate
Mar 19, 2026 9:35 PM UTC

Yes, that perfectly answers my question! Thank you very much for the clear explanation.

It is great to know that the pins can safely handle the high voltage if needed, but I will configure my voltage divider to provide around 4.7V to 5V for the deactivated state and 0V for the activated state, exactly as you recommended.

I really appreciate your help!