Skip to main content
Shane Kent
Associate II
November 3, 2023
Question

TCPP02-M18 - Spurious over-current protection fault occurs.

Hello - 

My team and I are utilizing the TCPP02-M18 in combination with the TI TPS65987 USB-C Controller in a USB Power Provider application.  

Right at the moment when a transition from the nominal 5V to a higher negotiated voltage occurs the TCPP02-M18 triggers an over-current fault and removes power from the Sink device. This is confirmed by reading the I2C registers of the TCPP02-M18 where Register 0x02 reports 0x82. When I clear the fault via the I2C writes the same cycle occurs.  

If I short over the sense resistor, R21 in our schematic, the over-current fault doesn't occur. Page 9 of the UM2973 for the X-NUCLEO-SRC1M1 suggests that the drain-to-gate capacitance for the MOSFET must be greater than 20pF.  I'm using the Vishay SQJQ904E-T1_GE3 as the dual N-Channel MOSFET in the provider path which has a gate capacitance of ~0.5nF to 1.5nF, so an additional capacitor should not be necessary.

The Sink device that I'm using in these tests on consumes ~20mA on the VBUS net, so we should be very far from any real overcurrent events. I do not see any transition events on the IANA output of the TCPP02-M18 that would indicate an overcurrent is actually occurring.

Below is a screenshot of the TCPP02-M18 portion of our schematic.

ShaneKent_0-1698970477505.png

Do you have any guidance or suggestions on how to continue to debug this?

- Shane

This topic has been closed for replies.

3 replies

Associate II
September 25, 2025

Hi Shane, 

Did you find an answer to this? or resolved this? We are facing the same issue. Thanks !

 

Shane Kent
Associate II
September 30, 2025
Hello -

No, unfortunately we did not get an answer to this question and to resolve
it we designed the TCPP02-M18 from our solution. It's a shame that ST does
not seem to prioritize support for these types of issues.

- Shane
Associate II
October 14, 2025

Hi Shane,

Here’s what we found:

The overcurrent events were indeed valid OCPs, confirmed by measuring the current across the shunt and with a current probe. Previously, we were monitoring the IANA pin output, but it did not capture the 200 us surge. I’d recommend checking the output using a current probe instead of relying on the IANA pin signal.

It is not some spike but the device (laptop) actually draws a surge for 200us.