Skip to main content
navid_nikoonasiri
Visitor II
Dec 21, 2016 10:03 AM UTC
Question

switching ADC with multi channel

Posted on December 21, 2016 at 11:03

Dear all

I am using ADC in stm8s105c6. I use ADC1 for two channel for example AIN9 and AIN8.

the problem is that when I switch the ADC1 from channel 9 to 8 the output result of the are being swapped.

the input signal which is connected to the channel 9 gives the result of the input signal which is connected to channel 8 and vice versa.

this the code that use.

     ADC1->CSR &= 0x00;

     ADC1->CSR |= 0x09;

     TIM1_SetCompare1(sample_average(pch1));

     

     ADC1->CSR &= 0x00;

     ADC1->CSR |= 0x08;

     TIM1_SetCompare2(sample_average(pch2));

(but when I use just one channel everything is ok);

Many Thanks for your help.

https://community.st.com/people/56065

‌
    This topic has been closed for replies.