Skip to main content
at1
Associate II
Nov 30, 2015 9:22 AM UTC
Question

SWIM sequence - recalibration after OPT Loading?

Posted on November 30, 2015 at 10:22

Hi,

I am implementing SWIM Protocol for an own programmer.

It already works quite well with STM8S003 but I am facing difficulties with STM8L101.

I wonder why the 128 HSI-timing-pulse on SWIM entry from the STM8L is ~85us long (I would expect 64us).

I wonder if this is because the HSIT bit in SWIM_CSR is not set during reset and the hsi is not calibrated before OPT loading.

Does the STM8L trim the HSI after reset-release (which includes OPT-loading) and therefore change the SWIM-clock speed?

So do I need to recalibrate my SWIM timing after stm8 option bytes have been loaded by cpu after reset-release?

My STM8S005 show similar behaviour. The STM8S003 I have tested are older production and STM8L und STM8S005 are ''fresh''. I did not check the issue on new STM8S003 yet - maybe it is similar..?

Thanks & best regards,

Alex

#swim
    This topic has been closed for replies.